|
|
 |
MAEC TOOL NEWS:
MAECT-PDSDKCOM-020801D
Emulator/Simulator Debugger Customizing Kit PDSDK COM KIT Released (English Version)
|
We have released emulator/simulator debugger customizing kit PDSDK COM KIT (English Version).
Notice:
The PDSDK COM KIT has been released on condition that no technical support for it, as well as for COM itself and development tools of Windows applications supporting COMs, can be provided. So, please be aware that if you put questions about these to us, we might not be able to answer them depending on your questions.
- Outline
The PDSDK COM KIT is used for expanding your debugger's functions.
- You can expand your debugger's functions using this kit as well as using conventional custom builders CBxx and CBxxSIM.
- Using commercially available Windows' application development tools (such as Microsoft's Visual Basic and Visual C++) that support COMs*, you can create application programs (for customizing windows, for example) and exchange data between different application programs.
| *: |
COM (Component Object Model), proposed by Microsoft, is a standard for combining application programs with each other. |
- Debuggers Supported
The PDSDK COM KIT supports the following debuggers:
- (1) Simulator debuggers
- M32C/80 and M16C/80 series MCUs
- M3T-PD308SIM V.3.00 Release 1
- M3T-PD308SIM V.3.00 Release 2
- M16C/60, M16C/30, M16C/20, and M16C/10 series MCUs
- M3T-PD30SIM V.5.00 Release 1
- (2) Emulator debuggers
- M32R family MCUs
- M3T-PD32R V.3.00 Release 1
- M32C/80 series MCUs
- M3T-PD308F V.1.00 Release 1
- M32C/80 and M16C/80 series MCUs
- M3T-PD308 V.3.00 Release 1
- M16C/60, M16C/30, M16C/20, and M16C/10 series MCUs
- M3T-PD30 V.6.00 Release 1
- 79xx series MCUs
- M3T-PD79 V.4.00 Release 1
- 77xx series MCUs
- M3T-PD77 V.4.00 Release 1
- 740 family MCUs
- M3T-PD38 V.5.00 Release 1
- Examples of Major Uses
- You can make a pseudo-target system to simulate your program's operation by using GUI parts available on the Windows' application development tools, which will facilitate the debugging of the completed target board.
- You can write the contents of your MCU's memory into a spreadsheet in Excel to analyze them. So, the results of analyses will easily be documented for evaluation.
- How to Get the Product
Please download the install program of the PDSDK COM KIT.
The Japanese version is also already downloadable.
- How to Use the Product
For information about how to use PDSDK COM KIT, see the reference manual and release note included with the product. The reference manual can be downloaded.
The Japanese version is also already downloadable.
- Provision of Sample Programs
We are releasing sample programs in succession on our tool home page.
|
 |