Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M3T-PD308F-020801D

Emulator Debugger M3T-PD308F
Upgraded to V.2.00 Release 1

We have upgraded emulator debugger M3T-PD308F for the M32C/80 series MCUs from V.1.00 Release 1 to V.2.00 Release 1.


  1. Descriptions of Upgrade
    1.1 New Features
    (1) IAR's EWM32C C++ debugging function supported.
    (2) Introduced the MIX display mode capable of simultaneously displaying execution instructions and accessed data in the Trace window.
    (3) Source codes, filenames, and line numbers can be typed when trace data in the Trace window is saved in text format.
    (4) Introduced the function of placing the addresses of the specified lines in the program counter (PC) in the Source and Program windows.
    (5) Introduced the function of displaying in the Program window the locations of the breakpoints selected in the S/W Breakpoint Setting window and the Address Interrupt Break window.
    (6) The communications interface in use can be displayed on the status bar.
    (7) When USB is used as a communications interface, an emulator can be selected among two or more emulators connected to USB ports of the host machine.
    (8) The user-defined clock (the clock internally generated in PC7501 based on the user-specified frequency) can be selected as the source of the main clock.
    (9) Supported the debugging of user programs written in the CPU rewrite mode in flash memory.

    1.2 Problems Fixed
    The following known problems have been fixed:
    (1) On setting search paths for source files:
    Even when a search path is set using the Customize dialog box or the Path script command, the source file located by the search path may not be displayed in the Program windows and others.
    For details, see MAEC TOOL NEWS "M3T-PD32RSIM, M3T-PD308SIM, M3T-PD30SIM, M3T-PD79SIM, M3T-PD77SIM, M3T-PD38SIM, M3T-PD32R, M3T-PD308, M3T-PD30, M3T-PD79, M3T-PD77, M3T-PD38, PD308M, and PD30M Precautions" issued on December 16, 2001.
    (2) On debugging functions in C language:
    During debugging in C language, Windows' error message may appear, resulting in the emulator debugger being terminated forcefully.
    For details, see MAEC TOOL NEWS "A Note on Emulator Debugger M3T-PD308F V.1.00 Release 1" issued on May 1, 2002.
    (3) On setting software breakpoints within the internal ROM area during execution of target programs
    (4) On step execution of the ldc instruction and setting software breakpoints in the emulator system on which a 2.0-cut version of the M32C/83 group MCU is mounted.

    Note:
    Problem (4) can be solved by using the firmware included with the upgraded M3T-PD308F product in combination with the emulator system concerned on which a 3.0-cut version of the M32C/83 group MCU is mounted.
    For information on the emulation systems on which a 3.0-cut version MCU is mounted, see the MAEC TOOL NEWS "Free-of-Charge Upgrade of MCU on Emulation Probe M30830T-EPB (Specific Product)" and "New Emulation Pod M30830T-RPD-E" issued on July 1, 2002.

  2. How to Upgrade Current Product and Order Upgraded One
    2.1 Online Upgrade (without Charge)
    Please download the upgraded product from HERE

    2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
    Upgrade service in CD-ROM is also available. When you place an order, please furnish the following information to your local Renesas Technology sales office or distributor:

    [First Ordering]
    Product Type:M3T-PD308F
    Version No.:V.2.00
    Release No.:Release 1
    -----
    Language:English
    -----
    Host OS: Windows XP, Windows Me, Windows 98, Windows 95, Windows 2000, or Windows NT 4.0

    [Upgrading by CD-ROM]
    Please let us know your product's license ID or serial number besides the above information.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal