Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M3T-SRA74-020801D

Relocatable Assembler M3T-SRA74 (for Windows)
Upgraded to V.4.10 Release 1A

We have upgraded the Windows version of relocatable assembler M3T-SRA74 for the 740 family MCUs from V.4.10 Release 1 to V.4.10 Release 1A.


  1. Description of Upgrade
    1.1 Improving the Installer
    At installing M3T-SRA74 V.4.00 Release 1 or later (for Windows), incorrect environment variable INC74 is set. This problem has been fixed by improving the installer in the upgraded product, so correct environment variable INC is properly set now.
    For details of this problem, see MAEC TOOL NEWS "A Note on Relocatable Assembler M3T-SRA74" issued on May 1, 2002.
    Note that only the installer has been upgraded in M3T-SRA74 V.4.10 Release 1A; the other items of software included in M3T-SRA74 remain intact.

  2. How to Upgrade Current Product and Order Upgraded One
    2.1 Online Upgrade (without Charge)
    Please download the upgraded product from HERE

    2.2 Upgrading by CD-ROM (with Additional Charge)
    Upgrade service in CD-ROM is also available. When you place an order, please furnish the following information to your local Renesas Technology sales office or distributor:

    Product Type:M3T-SRA74
    Version No.:V.4.10
    Release No.:Release 1A
    -----
    Language:English
    -----
    Host OS: Windows XP, Windows Me, Windows 98, Windows 95, Windows 2000, or Windows NT 4.0




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal