Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M3T-PD79-020916D

Emulator Debuggers
M3T-PD79, M3T-PD77, and M3T-PD38
Upgraded to V.4.10 Release 1, V.4.10 Release 1,
and V.5.10 Release 1 Respectively

We have upgraded emulator debuggers M3T-PD79, M3T-PD77, and M3T-PD38 as follows:
  • M3T-PD79 V.4.10 Release 1 for the 79xx series of MCUs
  • M3T-PD77 V.4.10 Release 1 for the 77xx series of MCUs
  • M3T-PD38 V.5.10 Release 1 for the 740 family of MCUs


  1. Descriptions of Upgrade
    1.1 New Feature
    When USB is used as a communications interface, an emulator can be selected out of two or more emulators connected to USB ports of the host machine.

    1.2 Problem Fixed
    (1)On debugging target programs during execution of them:
    If you try to open dialog boxes for setting breakpoints and changing windows etc., during execution of target programs, those dialog boxes may not appear, and the subsequent operations become frozen.
    For details, see MAEC TOOL NEWS "PD32RSIM, PD308SIM, PD30SIM, PD79SIM, PD77SIM, PD38SIM, PD32000, PD32R, PD308, PD30, PD79, PD77, PD38, PD308M, and PD30M Precautions" issued on May 16, 2001.
    (2)On opening source files in the Program and Source windows:
    In these windows, the symbol " - " does not appear in the BRK field, so that breakpoints cannot be set, or the MIX and DIS modes cannot be switched from the SRC mode.
    For details, see MAEC TOOL NEWS "PD308 V.3.00 Release 1, PD30 V.6.00 Release 1 and PD79 V.4.00 Release 1 Precautions" issued on May 16, 2001.
    (3)PD38 cannot be set up when used in combination with emulation pod M37207T-RPD for the 7200 series MCUs:
    When PD38 is used in combination with emulation pod M37207T-RPD, clicking the OK button in the Init dialog box opened at starting PD38 does not allow further set-up with an error message being displayed.
    For details, see MAEC TOOL NEWS "PD38 Precaution" issued on July 16, 2001.
    (4)On using the C Watch window:
    When variables are entered in the C Watch window, debuggers may be terminated forcibly.
    For details, see MAEC TOOL NEWS "PD32RSIM, PD308SIM, PD30SIM, PD79SIM, PD77SIM, PD38SIM, PD32000, PD32R, PD308, PD30, PD79, PD77, PD38, PD308M, and PD30M Precautions " issued on August 1, 2001.
    (5)On downloading target programs:
    If a Windows application is launched or any of the other already-opened Windows applications is made active while you are downloading a target program (a load module), the debugger may freeze suddenly.
    (6)On opening the Source window:
    The Source window may not be opened or not display materials normally if opened.
    (7)On setting search paths for source files:
    Even when a search path is set using the Customize dialog box or the Path script command, the source file located by the search path may not be displayed in the Program windows and others (M3T-PD79 only).
    For details of items (5), (6), and (7), see MAEC TOOL NEWS "M3T-PD32RSIM, M3T-PD308SIM, M3T-PD30SIM, M3T-PD79SIM, M3T-PD77SIM, M3T-PD38SIM, M3T-PD32R, M3T-PD308,M3T-PD30, M3T-PD79, M3T-PD77, M3T-PD38, PD308M, and PD30M Precautions" issued on December 16, 2001.

  2. How to Upgrade Current Products and Order Upgraded Ones
    2.1 Online Upgrade (without Charge)
    Please download the upgraded product you need from HERE

    2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
    Upgrade service in CD-ROM is also available. When you place an order, please furnish the following information to your local Renesas Technology sales office or distributor:

    [First Ordering]
    Product Type:
    Version No.:
    Release No.:
    -----
    Language:English
    -----
    Host OS: Windows XP, Windows Me, Windows 98, Windows 95, Windows 2000, or Windows NT 4.0

    [Upgrading by CD-ROM]
    Please let us know your product's license ID or serial number besides the above information.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal