|
|
 |
MAEC TOOL NEWS:
MAECT-M3T-NC308WA_2-020916D
A Note on C Compilers M3T-NC308WA V.5.00 Release 1 and M3T-NC30WA V.5.00 Release 1
|
Please take note of the following problem in using C compilers (with an assembler and integrated development environment) M3T-NC308WA and M3T-NC30WA:
- On describing an if or switch statement
- Products and Versions Concerned
- M3T-NC308WA V.5.00 Release 1
- for the M32C/80 and M16C/80 series of MCUs
- M3T-NC30WA V.5.00 Release 1
- for the M16C/60, M16C/30, M16C/20, and M16C/10 series of MCUs
- Description
When an auto variable storing a value is updated to another value in the program statement in an if or switch statement, the auto variable may not correctly be assigned to a register.
- Conditions
- This problem may occur if the following nine conditions are satisfied:
| (1) | Any one or more options are selected out of -O, -O[3-5], -OR, and -OS. |
| (2) | Option -ONBSD(-Ono_break_source_debug) is not selected. |
| (3) | An auto variable is assigned to a register. |
| (4) | An assignment expression "a" assigns a value to the auto variable in (3). |
| (5) |
There exists an if or switch selection statement, and its conditional expression evaluates the value that has been assigned to a register. |
| (6) | An assignment expression "b" that assigns a value to the auto variable in (3) exists in any of the program statements listed below. These program statements are written in the selection statement in (5)
| * | Either of the program statements for the if and else sections in an if-else statement. |
| * | The program statement for the if section in an if statement. |
| * | One or more, but not all, program statements for the case and default labels in a switch statement. | |
| (7) | The right term of the assignment expression "b" is the variable evaluated in the conditional expression in (5). |
| (8) | The auto variable in (3) is never referenced after the conditional expression in (5) until the assignment expression "b" in (6) started. |
| (9) | The auto variable in (3) is referenced after the selection statement in (5) ended. |
- Example
-----------------------------------------------------------
char gc,gc2;
void func(void)
{
-
a char c = 0; /* Condition (4) */
-
switch(gc){ /* Condition (5) */
case 1:
case 2:
-
b c = gc; /* Conditions (6) and (7) */
-
break;
default:
break;
}
if(c != 0){ /* Condition (9) */
gc2++;
}
}
-----------------------------------------------------------
- Workaround
- This problem will be circumvented in any of the following ways:
- (1) Compile programs after deselecting the -O, -O[3-5], -OR, and -OS options.
- (2) Use option -ONBSD(-Ono_break_source_debug).
- (3) Place a dummy asm function immediately before the if or switch statement.
[Example]
-----------------------------------------------------------
char gc,gc2;
void func(void)
{
char c = 0;
asm(); /* A dummy asm function placed */
switch(gc){
case 1:
case 2:
c = gc;
break;
default:
break;
}
if(c != 0){
gc2++;
}
}
-----------------------------------------------------------
- Schedule of Fixing the Problem
For M3T-NC308WA, we plan to fix this problem in our next release.
For M3T-NC30WA, the problem has been fixed in its V.5.00 Release 2.
|
 |