|
|
 |
MAEC TOOL NEWS:
MAECT-IODLL-021001D
Simulator Debugger Customizing Kit PDxxSIM I/O DLL KIT Released (English Version)
|
We have released simulator debugger customizing kit PDxxSIM I/O DLL KIT (English version).
Notice:
This product has been released on condition that no technical support for it can be provided, as well as for Windows' application development tools supporting DLLs. So, please be aware that if you put questions to us, we might be unable to answer them depending on your questions.
- Description
- Customizing kit PDxxSIM I/O DLL KIT for simulator debugger M3T-PDxxSIM facilitates the creation of I/O DLLs*. M3T-PDxxSIM can operate PDxxSIM I/O DLL KIT loaded in it synchronized with timing of single-step execution, reads from/writes to memory, interrupt requests, and so on.
- Notice:
To create I/O DLLs, you need to use a commercially available Windows' application development tool--Microsoft Visual C++.
| * |
DLL, the acronym for Dynamic Link Library, is a function of the operating system that enables you to save executable routines (those providing a specific function or a collection of specific functions) as files given filename extension .dll. These routines are read in only when called from the program that needs them. |
- Simulator Debuggers Supporting PDxxSIM I/O DLL KIT
The following version and later of the simulator debuggers support PDxxSIM I/O DLL KIT:
- M32C/80 and M16C/80 series of MCUs
- M3T-PD308SIM V.3.00 Release 2
- M16C/60, M16C/30, M16C/20, and M16C/10 series of MCUs
- M3T-PD30SIM V.5.00 Release 1
- Examples of Major Uses
- You can simulate the I/O ports or the operations of on-chip peripheral functions of the target MCU to verify your program execution.
- By calling the interface with Microsoft Excel from the kit, you can read the input data to a port from files in Excel or write the output data from a port into files in Excel to analyze the results of the output.
- How to Get the Product
Please download the install program of PDxxSIM I/O DLL KIT.
The Japanese version is also already downloadable.
- How to Use the Product
See the User's manual and release note included with PDxxSIM I/O DLL KIT. The User's manual in PDF can be downloaded.
The Japanese version is also already downloadable.
|
 |