|
|
 |
MAEC TOOL NEWS:
MAECT-M3T-PD30F-021016D
New Emulator Debugger M3T-PD30F V.1.00 Release 1
|
We have released new emulator debugger M3T-PD30F V.1.00 Release 1 for the M16C/60 series of MCUs.
- Outline
M3T-PD30F is an emulator debugger for Mitsubishi's M16C/60 series of microcomputers used in combination with emulator PC7501 for the M16C MCU family.
M3T-PD30F provides versatile debugging functions that make PC7501 reach its full potential, as well as user-friendly GUI (Graphical User Interface). So it can deliver outstanding performance of debugging application programs and target systems.
- Features
- M3T-PD30F has the following features:
- (1) Supporting PC7501 with the following improved functions:
- Real-time RAM monitoring area: 4 KB (16 blocks of 256 bytes)
- Real-time trace: 256 kilocycles measurable
- Hardware breakpoints and trace points: 8 points settable each
- (2) Supporting emulation probe M3062PT-EPB for the M16C/62P group.
Note, however, that the probes manufactured as specific products (ES) cannot be used in combination.
- (3) Keeping the same functionality and operability as those of emulator debugger M3T-PD308F (V.2.00 Release 1) used with PC7501.
- For more details, please go to the data sheet.
- Ordering Information
When you place an order of M3T-PD30F, please contact your local Renesas Technology sales office or distributor.
| Product Type | : | M3T-PD30F |
| Version No. | : | V.1.00 |
| Release No. | : | Release 1 |
| ----- |
| Language | : | English |
| ----- |
| OS | : |
Windows XP, Windows Me, Windows 98, Windows 95, Windows 2000, or Windows NT 4.0 |
- To the customer who is using M3T-PD30F V.1.00 ES1
- Please use M3T-PD30F V.1.00 ES1 as it is until we inform you when to upgrade it to M3T-PD30F V.1.00 Release 1.
- M3T-PD30F V.1.00 Release 1 for the M16C/60 series cannot be used in combination with the ES version of M3062PT-EPB. In such a case, use M3T-PD30F V.1.00 ES1 together with it.
|
 |