Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M3062PT-EPB-021016D

Emulation Probe
M3062PT-EPB (Specific Product) Released

We have released emulation probe M3062PT-EPB (specific product), dedicated to emulator PC7501, for the M16C/62P MCUs of the M16C/62 group in the M16C/60 series.


  1. Outline
    M3062PT-EPB is an emulation probe used in combination with emulator PC7501 for the M16C family MCUs.
    For details of PC7501, please see the data sheet.

    The product released this time, on which evaluation MCU M30627FHPGP (2.4 cut) is mounted, supports the M16C/62P MCUs of the M16C/62 group in the M16C/60 series. Its operating conditions are as follows:
    • Maximum operating clock frequency: 24 MHz (at Vcc = 3.0--5.5 V)
    • Power supply to the target system: 2.7--5.5 V

    The Contents of the Product Package:
    • Two MCU boards M3062PT-EPBM and M3062PT-EPBD for the M16C/62P MCUs of the M16C/62 group
    • An evaluation MCU M30627FHPGP (2.4-cut version, already mounted)
    • A probe board PCA7501EPBA for PC7501 (supporting the M16C/60 series)
    • A converter M30800T-PTC for connecting M3062PT-EPB to a 100-pin 0.65-mm-pitch QFP
    • An instruction manual

    For further information about these contents, please go to the data sheet.

  2. Ordering Information
    Product TypeType NameComment
    M3062PT-EPBM3062PT-EPB--

  3. Note on the Specific Product
    The product released this time is a specific product on which a 2.4-cut ES version of the evaluation MCU is mounted. We will inform you at a later date on the news when to replace the already-mounted MCU with the upgraded one free of charge.

  4. To the customer who is using the ES version of M3062PT-EPB
    • Please use the ES version of M3062PT-EPB as it is until we inform you when to replace the 2.1-cut version of the evaluation MCU with the upgraded one.
    • M3T-PD30F V.1.00 Release 1 for the M16C/60 series cannot be used in combination with the ES version of M3062PT-EPB. In such a case, use M3T-PD30F V.1.00 ES1 together with it.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal