Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M34502T-MCU-021201D

A Note on MCU Board M34502T-MCU

Please take note of the following problem in using MCU board M34502T-MCU for the 4501, 4502, 4506, 4507, and 4580 groups in the 4500 series MCUs:
  • On using the P12/CNTR pin as the input pin of CNTR signals


  1. Product Concerned
    M34502T-MCU

  2. Description
    When the P12/CNTR pin of the M34502T-MCU board is used as the input pin of the event-counting clocks to timer 2 (that is, as the timer input pin), clocks cannot properly be counted.

    Notes:
    1. This problem arises only in the emulator and does not in the actual MCU.
    2. This problem does not arise when the P12/CNTR pin is used as the P12 I/O port pin or the output pin of CNTR signals (as the timer output pin).

  3. Temporary Solution
    When you want to debug and evaluate target systems that need timer input, please use the OTP version of the target MCU instead of the M34502T-MCU board.

    The schedule of fixing this problem will be notified on MAEC TOOL NEWS at a later date when made up.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal