Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-TM-021216D

Information on Releasing
the Function-Enhancing Patch Tool for TM V.3.20
Included with the Windows' Versions of
C Compilers M3T-CC32R, M3T-NC308WA, and M3T-NC30WA

We are releasing the patch tool for enhancing the function of scanning the dependencies of header files on a source file in integrated development environment TM V.3.20.

  1. Feature of the Patch Tool
    The patch tool to be released enhances the function of scanning the dependencies of files as follows:
    Previously, the dependencies of included files on a source file have been created by making effective the lines containing the #include preprocessor-directive statement in C language.
    After the scanning function has been enhanced, on the contrary, the dependencies of files are created by excluding the #include statements contained in the lines that become ineffective within the #if--#else--#endif block.
    This change enables you to obtain the list of the include files dependent on a source file more correctly.

    1.1 Products and Versions Concerned
    The patch tool can be used in the TM V.3.20 contained in the following C compiler products and their versions:
    • M3T-CC32R V.2.10 Release 1--V.4.00 Release 1 (Windows version only)
    • M3T-NC308WA V.3.00 Release 1--V.3.10 Release 3 (Windows version only)
    • M3T-NC30WA V.4.00 Release 1--V.5.00 Release 2 (Windows version only)

    1.2 Source Files Concerned
    The dependencies of header files on the following source files are scanned:
    (1)For M3T-CC32R
    C source files (Assembly source files are excluded.)
    (2)For M3T-NC308WA and M3T-NC30WA
    C and assembly source files

  2. How to Get and Install the Patch Tool
    (1)Download the patch tool (tmv3patch_e.exe: 761KB).
    (2)When TM is running, close it.
    (3)Execute the downloaded tmv3patch_e.exe file; then the installer will be invoked.
    (4)Install the patch tool according to the installer's instructions.

    [NOTICES:]
    • This patch tool enhances the scanning function by making changes to the settings on the cross tool, not on the TM.
      So, the patch tool must be executed each time a cross tool is installed since it has no effect on cross tools that are only installed after a run of patch tool.
    • To uninstall cross tools for which the patch tool has ever been executed, be sure to uninstall "Product Type TM V.3 Information" first.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal