Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M3062PT-EPB_1-030216D

Emulation Probe M3062PT-EPB Released

We have released the PC7501-dedicated emulation probe M3062PT-EPB for the M16C/62P MCU in the M16C/62 group of the M16C/60 series.


  1. Outline
    The M3062PT-EPB is an emulation probe used together with the PC7501 emulator for the M16C family MCUs. For details of this product, please see its data sheet.

    The product released this time, on which the production-run evaluation MCU M30627FHPGP is mounted, can support the M16C/62P MCU in the M16C/62 group of the M16C/60 series.
    The product is capable of operating at the following conditions:
    • Maximum clock frequency: 24 MHz (within a Vcc range of 3.0--5.5 V)
    • Supply voltage to target MCU: 2.7--5.5 V

    The Contents of the Product Package:
    1. An MCU board--M3062PT-EPBM--for the M16C/62P in the M16C/62 group
    2. An evaluation MCU--M30627FHPGP (already mounted)
    3. A probe board--PCA7501EPBA--for the PC7501
    4. A conversion board--M30800T-PTC--for connecting M3062PT-EPBM to a 100-pin 0.65-mm-pitch QFP
    5. A 100-pin LCC socket--IC61-1004-051--manufactured by Yamaichi Electronics Co., Ltd.
    6. Oscillator boards
      OSC-3 for the 16-MHz main clock
      OSC-2 for the main clock
    7. Six resistor arrays--eight 51-k ohms resistors each--for pulling up ports P0 through P5
    8. A user's manual

    For further information on the package, please go to the data sheet.

  2. Ordering Information
    Product TypeType NameComment
    M3062PT-EPBM3062PT-EPB-

  3. Upgrade of the M3062PT-EPB Fabricated as ES and Specific Products
    On the M3062PT-EPB fabricated as ES and specific products is mounted the ES-version MCU.
    For information on free-of-charge upgrade of this probe to the type of newly released one, see MAEC TOOL NEWS "Free-of-Charge Upgrade of the M3062PT-EPB Emulation Probe Fabricated as ES and Specific Products"" issued on February 16, 2003.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal