Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS [RSO-M34519T2-CPE-030401D]

Compact Emulator M34519T2-CPE
Released

We have released the M34519T2-CPE compact emulator for the 4518, 4519, 4583, and 4584 groups in the 4500 series MCUs.


  1. Outline
    The M34519T2-CPE, though compact in size and low-priced, comes with such software tools as an assembler and emulator debugger and provides the debugging functions identical to the PC4504 emulator system.
    Its features are as follows:
    • The dimensions of the emulator body are 120 mm in width, 85 mm in depth, and 32 mm in height.
    • USB is used as a communications interface.
    • The M3T-PD45M emulator debugger for the product's exclusive use is included with the package.

    For detailed specifications of the product, see its data sheet.

  2. Ordering Information
    Product TypeType NameComment
    M34519T2-CPEM34519T2-CPE-
    NOTICE:
    At this moment, the M34519T2-CPE cannot be shipped to the countries that require electronic gear should bear the CE mark.
    So please restrain from shipping it to those countries for a while until we complete the formalities of applying for the mark.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal