Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS [RSO-M3T-PD30F-030401D]

A Note on Using Emulator Debugger
M3T-PD30F V.1.00 Release 1

Please take note of the following problem in using the M3T-PD30F emulator debugger for the M16C/60 series MCUs:
  • On using the MR trace window


  1. Version Concerned
    M3T-PD30F V.1.00 Release 1

  2. Description
    When the MR trace window is opened to display the execution history of a task, the error message saying "Interrupt handler issued a system call that can be issued from only tasks." may appear, resulting in the incorrect execution history being displayed.
    2.1 Conditions
    This problem occurs if fetching the reit instruction executed in a system call and writing data into OS's resource by the M3T-MR30 are performed in the same cycle.

  3. Workaround
    This problem can be circumvented by using the problem-fixed DLL file.
    So, please replace the DLL file in your product with the above-mentioned one as follows:
    (1)Download the problem-fixed DLL file, p30frtoswin.exe (187KB).
    (2)Decompress the downloaded file to obtain the p30fRTOSWin.dll file (V.1.10.10).
    (3)With the decompressed file, overwrite the old p30fRTOSWin.dll file in the folder where the M3T-PD30F resides.
    (4)Confirm the version of the new DLL file as follows:
    (a)Launch the M3T-PD30F.
    (b)Open the Help menu and select About; then the Version dialog box opens, on which the version of the problem-fixed DLL file will be displayed.
    (c)Confirm the version is V.1.10.10.

  4. Schedule of Fixing the Problem
    We plan to fix this problem in our next release of the product.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal