Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS [RSO-PDSDKCOM-030501D]

Emulator/Simulator Debugger Customizing Kit
PDSDK COM Kit
V.1.10 Upgraded

We have upgraded the PDSDK COM emulator/simulator debugger customizing kit from V.1.00 to V.1.10.
NOTICE:
This product has been released on condition that no technical support for it can be afforded, as well as for COM itself and development tools of Windows applications supporting COMs. So, please be aware that if you put questions to us, we might be unable to answer them depending on your questions.


  1. Descriptions of Upgrade
    1.1 Improvements Introduced
    (1)Supporting the M3T-PD32RM emulator debugger, which is used in conjunction with the M32100T3-SDI-E or M32100T-EZ-E emulator for the M32R family MCUs.
    (2)Providing the following methods.
    MethodDescription
    sym_get_obj_nameGets an object name
    sym_get_src_nameGets a source-file name
    sym_get_func_nameGets a function name
    sym_get_func_infoGets information on a function
    sym_get_variable_infoGets information on a C variable
    info_get_debuggerGets the model name of a debugger
    info_get_mcufile_nameGets the name of the MCU file selected
    err_get_messageGets an error message string

    The above methods can be used in the following debuggers:
    • M3T-PD32RM V.1.00
    • M3T-PD308F V.3.00
    • M3T-PD308 V.5.00
    • M3T-PD308SIM V.3.10
    • M3T-PD30F V.2.00
    • M3T-PD30 V.8.00
    • M3T-PD30SIM V.5.10
    (3)Providing the SFR window function as one of sample programs. This window function can run on the following debuggers:

    Emulator debuggers used with the PC7501 emulator:
    • M3T-PD308F V.1.00 or later for the M32C/80 and M16C/70 series MCUs
    • M3T-PD30F V.1.00 or later for the M16C/60 series MCUs
    Emulator debuggers used with the PC4701 emulator:
    • M3T-PD308 V.3.00 or later for the M32C/80 and M16C/80 series MCUs
    • M3T-PD30 V.6.00 or later for the M16C/60, M16C/30, M16C/20, and M16C/10 series MCUs
    Simulator debuggers:
    • M3T-PD308SIM V.3.00 or later for the M32C/80 and M16C/80 series MCUs
    • M3T-PD30SIM V.5.00 or later for the M16C/60, M16C/30, M16C/20, and M16C/10 series MCUs
    NOTICE:
    When you use the PDSDK COM kit, ensure that your debugger is of the latest version.

    1.2 Problems Fixed
    The following known and newly found problems have been fixed:
    (1)On creating custom windows calling such "methods" as sym_val2sym, sym_val2bit, and sym_get_scope by using PDSDK COM KIT
    For details, see MAEC TOOL NEWS "Note on Emulator/Simulator Customizing Kit PDSDK COM KIT" issued on October 1, 2002.
    (2)On creating a custom window calling the mem_set_multi method by using PDSDK COM KIT on M3T-PD79, M3T-PD77, and M3T-PD38.

  2. How to Upgrade the Current Product
    2.1 Online Upgrade (without Charge)
    Please download the upgraded product from HERE.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal