Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS [RSO-M3T-PD308SIM-030501D]

Simulator Debuggers
M3T-PD308SIM, M3T-PD30SIM, M3T-PD79SIM, M3T-PD77SIM, and M3T-PD38SIM
Upgraded

We have upgraded simulator debuggers. The upgraded products and their versions are as follows:
  • M3T-PD308SIM V.3.10 Release 1 for the M32C/80 and M16C/80 series MCUs
  • M3T-PD30SIM V.5.10 Release 1 for the M16C/60, M16C/30, M16C/20, and M16C/10 series MCUs
  • M3T-PD79SIM V.3.20 Release 1 for the 79xx series MCUs
  • M3T-PD77SIM V.3.10 Release 1 for the 77xx series MCUs
  • M3T-PD38SIM V.2.10 Release 1 for the 740 family MCUs


  1. Descriptions of Upgrade
    1.1 Improvements Introduced
    • To the M3T-PD77SIM only:
      (1)Supporting source-level debugging of source programs in assembly language when IAR Systems' ICC7700 C compiler (Embedded Workbench EW7700) is used.
    • To the M3T-PD38SIM only:
      (1)Supporting source-level debugging of source programs in assembly language when IAR Systems' ICC740 C compiler (Embedded Workbench EW740) is used.

    1.2 Problems Fixed
    The following known and newly found problems have been fixed:

  2. How to Upgrade the Current Products and Order the Upgraded Ones
    2.1 Online Upgrade (without Charge)
    Please download the upgraded product you want from HERE.

    2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
    Upgrade service in CD-ROM is also available. When you place an order please furnish the following information to your local Renesas Technology sales office or distributor:

    [First Ordering]
    Product Type:
    Version No.:
    Release No.:
    Host OS: Windows XP, Windows Me, Windows 98, Windows 95, Windows 2000, or Windows NT 4.0

    [Upgrading by CD-ROM]
    Please let us know your product's license ID or Serial No. besides the above information.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal