|
|
 |
RENESAS TOOL NEWS [RSO-PCA7750G02-030616D]
Pitch Converter Boards PCA7750G02-BARE and PCA7750G02 Released
|
We have released the PCA7750G02-BARE and PCA7750G02 boards for converting pitches from 0.8 mm to 2.54 mm (standard pitch).
- Outlines
- 1.1 PCA7750G02-BARE
- As a pitch converter, this board enables you to connect an MCU encapsulated in the 80P6N-A or 80D0 package to the standard 2.54-mm-pitch universal board, which is useful in prototyping.
On the board is printed a foot pattern used for either the 80-pin 0.8-mm-pitch QFP package (80P6N-A) or the 80-pin 0.8-mm-pitch LCC one (80D0), and on the pattern can be mounted any of the following IC sockets for accommodating an MCU in the 80P6N-A or 80D0 package. (See Notes 1 and 2.): * MCU of the 80P6N-A package can be mounted directly on the pattern.
- MCU of the 80P6N-A package manufactured by Renesas Technology Corp.
- IC61-080-079 for 80D0 (surface mounted LCC),
- IC61-080-081 for 80D0 (hand-soldered LCC), and
- IC61-0804-046 for 80D0 (hand-soldered LCC) manufactured by Yamaichi Electronics Co., Ltd.
- AXS4803M19 for 80P6N-A (QFP) manufactured by Matsushita Electric Works, Ltd.
- NQPACK080RA (converter board) for 80P6N-A (QFP) manufactured by Tokyo Eletech Corporation
- Notes:
- The PCA7750G02-BARE is the modified product of the current PCA7750-BARE such a way that the latter's foot pattern is redesigned to accept the AXS4803M19 and NQPACK080RA QFP sockets.
- When you use MCU of the 80D0 package, please mount any of the above-listed LCC sockets for it instead of mounting directly MCU on the pattern.
- 1.2 PCA7750G02
- This converter board consists of a PCA7750G02-BARE board and an 80-pin 0.8-mm-pitch LCC socket already mounted on it. So an MCU encapsulated in the 0.8-mm-pitch LCC package (80D0) can easily be connected to the standard 2.54-mm-pitch universal board through this, which is useful in prototyping.
- Note that between the PCA7750G02 and the current PCA7750, there are no differences in their functions since they have an already-mounted LCC socket of the same type on their foot patterns.
- NOTICE:
- As stated above, there are no differences between the PCA7750G02 and the PCA7750 in their functions. So please be aware that if you place the order of a PCA7750G02 product, a PCA7750 may be delivered for some period of time.
- For more details, see the following datasheets.
- PCA7750G02-BARE
- PCA7750G02
- Ordering Information
| Product Type | Type Name | Comment |
| PCA7750G02-BARE | PCA7750G02-BARE | - |
| PCA7750G02 | PCA7750G02 | - |
|
 |