|
|
 |
RENESAS TOOL NEWS [RSO-PCA7752AG02-030616D]
Pitch Converter Boards PCA7752AG02-BARE and PCA7752AG02 Released
|
We have released the PCA7752AG02-BARE and PCA7752AG02 boards for converting pitches from 0.65 mm to 2.54 mm (standard pitch).
- Outlines
- 1.1 PCA7752AG02-BARE
- As a pitch converter, this board enables you to connect an MCU encapsulated in the 100P6S-A or 100D0 package to the standard 2.54-mm-pitch universal board, which is useful in prototyping.
On the board is printed a foot pattern used for either the 100-pin 0.65-mm-pitch QFP package (100P6S-A) or the 100-pin 0.65-mm-pitch LCC one (100D0), and on the pattern can be mounted any of the following IC sockets for accommodating an MCU in the 100P6S-A or 100D0 package. (See Notes 1 and 2.): * MCU of the 100P6S-A package can be mounted directly on the pattern.
- MCU of the 100P6S-A package manufactured by Renesas Technology Corp.
- IC61-1004-051 for 100D0 (LCC) manufactured by Yamaichi Electronics Co., Ltd.
- AXS4003M295C for 100P6S-A (QFP) manufactured by Matsushita Electric Works, Ltd.
- NQPACK100RB (converter board) for 100P6S-A (QFP) manufactured by Tokyo Eletech Corporation
- Notes:
- The PCA7752AG02-BARE is the modified product of the current PCA7752A-BARE such a way that the latter's foot pattern is redesigned to accept the AXS4003M295C and NQPACK100RB QFP sockets.
- When you use MCU of the 100D0 package, please mount any of the above-listed LCC sockets for it instead of mounting directly MCU on the pattern.
- 1.2 PCA7752AG02
- This converter board consists of a PCA7752AG02-BARE board and an 100-pin 0.65-mm-pitch LCC socket already mounted on it. So an MCU encapsulated in the 0.65-mm-pitch LCC package (100D0) can easily be connected to the standard 2.54-mm-pitch universal board through this, which is useful in prototyping.
- Note that between the PCA7752AG02 and the current PCA7752A, there are no differences in their functions since they have an already-mounted LCC socket of the same type on their foot patterns.
- NOTICE:
- As stated above, there are no differences between the PCA7752AG02 and the PCA7752A in their functions. So please be aware that if you place the order of a PCA7752AG02 product, a PCA7752A may be delivered for some period of time.
- For more details, see the following datasheets
- PCA7752AG02-BARE
- PCA7752AG02
- Ordering Information
| Product Type | Type Name | Comment |
| PCA7752AG02-BARE | PCA7752AG02-BARE | - |
| PCA7752AG02 | PCA7752AG02 | - |
|
 |