Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS [July 1, 2003: RSO-M3T-PD45M-030701D]

Debugger M3T-PD45M
Upgraded to V.1.10 Release 1

We have upgraded the M3T-PD45M debugger dedicated to the compact emulator for the 4-bit MCUs from V.1.00 Release 1 to V.1.10 Release 1.

  1. Descriptions of Upgrade
    1.1 Improved Function
    Target programs can be downloaded from the PC to the emulator at higher speeds.

    1.2 Problems Fixed
    The following known and newly found problems have been fixed:
    (1)The problems in using the M34519T2-CPE compact emulator
    For details, see RENESAS TOOL NEWS "Notes on Using Compact Emulator M34519T2-CPE" issued on July 1, 2003.
    (2)Problem causing the debugger to hang if a script command is executed in the Script window immediately after the program's halting

  2. Online Upgrade (without Charge)
    Please download the upgraded product from HERE.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal