Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS [September 1, 2003: RSO-SWTOOL-030901D]

Five Software Products Updated

We have updated five software products in their corporate name displayed at launching them since our corporate name was changed from Mitsubishi Electric Semiconductor Application Engineering Corporation to Renesas Solutions Corporation on this April 1.

For information on establishment of the latter company, visit the Web site.

  1. Updated Products
    1.1 Mask File Converter
    MM from V.3.00 Release 3 to V.3.00 Release 3A

    1.2 C Compilers
    M3T-NC79WA for the 7900 series MCUs from V.4.10 Release 1A to V.4.10 Release 1B
    M3T-NC77WA for the 77xx series MCUs from V.5.20 Release 4 to V.5.20 Release 4A

    1.3 Assemblers
    M3T-RASM77 for the 77xx series MCUs from V.5.10 Release 1 to V.5.10 Release 1A
    M3T-SRA74 for the 740 series MCUs from V.4.10 Release 1A to V.4.10 Release 1B


  2. Description
    The corporate name displayed at launching the above five software products has been updated. However, no specifications and functions of these updated products have been subject to any changes.

    NOTICE:
    When you have updated your compiler or assembler, you should upgrade the TM to its latest version at the same time if you want to run it on the updated compiler or assembler.


  3. How to Update the Current Products and Order the Updated Ones
    3.1 Online Update (without Charge)
    Please download the updated product you want from HERE.

    3.2 First Ordering or Updating by CD-ROM (with Additional Charge)
    Update service in CD-ROM is also available. When you place an order please furnish the following information to your local Renesas Technology sales office or distributor:

    [First Ordering]
    Product Type:
    Version No.:
    Release No.:
    -----
    Host OS: Windows XP, Windows Me, Windows 98, Windows 95, Windows 2000, or Windows NT 4.0

    [Updating by CD-ROM]
    Please let us know your product's license ID or Serial No. besides the above information.

    NOTICES:
    1. The integrated development environment TM cannot be purchased alone; it is included with each cross-tool product.
    2. The mask file converter MM cannot also be purchased; it can be downloaded from the Web site.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal