|
|
 |
RENESAS TOOL NEWS [September 16, 2003: RSO-M3T-MR30-030916D]
Real-Time OSes M3T-MR30 Upgraded to V.3.30 Release 2
|
We have upgraded the M3T-MR30 real-time OSes for the M16C/60, M16C/30, M16C/20 and M16C/10 series MCUs as follows:
- the M3T-MR30K real-time OS development kit: from V.3.30 Release 1 to V.3.30 Release 2
- the M3T-MR30S real-time OS mass-production contract: from V.3.30 Release 1 to V.3.30 Release 2
- Descriptions of Upgrade
- 1.1 New Features
-
- (1) Supporting the MISRA C rules(*)
- Using the -D__MISRA_C__ compile option can select the prototype declaration for the MISRA C rules.
- Note:
- * The MISRA C is Guidelines for the Use of the C Language in Vehicle Based software. They were prepared by a non-profit group MISRA (Motor Industry Software Reliability Association) organized by
Japan's automobile industry for software reliability promotion.
The guidelines lay down 127 rules regarding C-language programs for
automotive use.
- 1.2 Problems Fixed
- The following known problems have been fixed:
- (1) On using the iwup_tsk system call(*)
- (2) On using the -fansi option in the nc30 compiler
- For details of the above items, see MAEC TOOL NEWS "MR30 Precaution"
issued on August 1, 2001 and to see the products' datasheets.
- How to Update the Current Products and Order the Updated Ones
The M3T-MR30 is a product for special users. If you need the latest
version of Real-time OS with online, please contact RSO Tool Technical Support.
|
 |