|
|
 |
RENESAS TOOL NEWS [September 16, 2003: RSO-TM-030916D]
A Note on Using Integrated Development Environment TM
|
Please take note of the following problem in using the integrated
development environment TM:
- On scanning the dependencies of header files on a source file
- Versions Concerned
This problem occurs if a version of the TM is used in combination with
a specific compiler or assembler. The relations between them are shown in
the table below.
| TM | Compilers and Assemblers |
| V.3.20A | M3T-CC32R V.3.00 R1 through V.4.10 R1, M3T-NC308WA V.3.00 R1 through V.5.00 R1, and M3T-NC30WA V.4.00 R1 through V.5.00 R2 |
| V.3.00 through V.3.20(*) | M3T-CC32R V.3.00 R1 and later, M3T-NC308WA V.3.00 R1 and later, and M3T-NC30WA V.4.00 R1 and later |
| V.3.00 through V.3.20A | M3T-NC79WA V.4.00 R1 and later, M3T-NC77WA V.5.20 R4 and later, and M3T-SRA74 V.4.10 R1 and later |
| V.3.20 and V.3.20A | M3T-ICC740 V.1.00 R1 and V.1.00 R1A |
NOTE:
| * | The problem does not occur if the patch tool program for improving
the TM's functions is executed on the TM V.3.20. |
- Description
When the dependencies of header files on a source file are scanned,
the include files saved in the directory specified in the environment
variable INCxx cannot be searched for.
- Workaround
This problem can be circumvented in either of the following ways:
| (1) | Specify the relative or absolute path name of each header file written in the #include statement of a source file. |
| (2) | If the -I option is available which specifies directories where include files are searched for(*), use the directory specified in the environment variable INCxx as a parameter of this option. |
NOTE:
| * | All our compilers and assemblers provide the -I option except rasm77.exe in the M3T-NC77WA and sra74.exe in the M3T-SRA74. |
Example of Setting a parameter of the -I option in the M3T-NC30WA
| a. | Open Project Editor and select Project and then Option Browser
menu. You will see the Option Browser dialog box displayed. |
| b. | Select the CFLAGS option-macro and click the Edit button.
The Option dialog box appears. |
| c. | Select "Control of Compile Driver" out of Categories. |
| d. | Select the -I option and then click the Parameter button.
You see the Set Parameter dialog box. |
| e. | Type the directory name specified in the INCxx environment
variable into the text box. If you type two or more directories,
delimit them with commas. |
| f. | Click the OK buttons on all the dialog boxes. |
- Schedule of Fixing the Problem
We plan to fix this problem in our next release of the product.
|
 |