|
|
 |
RENESAS TOOL NEWS on October 16, 2003: RSO-TM-031016D
A Note on Using Integrated Development Environment TM
|
Please take note of the following problem in using the TM, an integrated development environment:
- On editing commands using the project editor
- Versions Concerned
TM V.3.20 -- V.3.20A
- Description
If a command is edited in the following steps, a link error that does not appear before editing may arise because the contents of the command file are not updated correctly (if a rebuild is executed, the TM works properly):
| (1) | The project editor is displayed. |
| (2) | The <Project name>.cmd file is opened in the project tree and then the "Project" -> "Edit item" -> "Command" menu is selected. |
| (3) | A command that includes no redirection character (> or >>) is placed in the first line of the command file in the Command dialog box.
|
- Workaround
Be sure to place a command that includes a redirection character (> or >>) in the first line of the command file.
- Schedule of Fixing the Problem
We plan to fix this problem in our next release of the product.
|
 |