Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on October 16, 2003: RSO-HEW-031016D

A Note on Using
Integrated Development Environment High-performance Embedded Workshop

Please take note of the following problem in using the High-performance Embedded Workshop, an integrated development environment.
  • On using the Import Makefile function


  1. Versions Concerned
    (1) High-performance Embedded Workshop Version 3.01 (release 1) bundled with the M3T-NC30WA V.5.20 Release 1
    (2) High-performance Embedded Workshop Version 3.01 (release 1) bundled with the M3T-NC30WA (Free version for R8C/Tiny only)


  2. Description
    The High-performance Embedded Workshop is unsuccessfully terminated when you use the High-performance Embedded Workshop in combination with the M3T-NC30WA V.5.20 Release1 and create a new High-performance Embedded Workshop work space in the following steps:
    (1) A <makefile> file is selected in the Makefile Path text box using the Import Makefile function of the New Project Work Space dialog box.
    (2) Then the Start button is clicked.


  3. Workaround
    Don't click the Start button.
    When a <makefile> file is selected in the Makefile Path text box, the High-performance Embedded Workshop immediately starts analyzing the makefile information. So you need not click the Start button.


  4. Schedule of Fixing the Problem
    We plan to fix this problem in our next release of the product.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal