|
|
 |
RENESAS TOOL NEWS on December 1, 2003: RSO-M3T-PD45M-031201D
|
MCU Data Files for the M3T-PD45M Emulator Debugger Supplied
|
We supply MCU data files for the M3T-PD45M emulator debugger (with an assembler) dedicated to the compact emulator for the 4500 series MCUs. These MCU data files have not yet been included with the debugger though they are necessary to developing programs for the H versions of 4552, 4553, and 4556 group MCUs.
- Versions Concerned
M3T-PD45M V.1.00 Release 1 and V.1.10 Release 1
- MCU Data Files Supplied
The following MCU data files are supplied. They can be used for developing programs for the H versions of the 4552, 4553, and 4556 group MCUs:
-
- MCU data files (DAT files)
| MCU | MCU Data File |
| M34552M4H-XXXFP | M4552M4H.DAT |
| M34553M4H-XXXFP | M4553M4H.DAT |
| M34556M4H-XXXFP | M4556M4H.DAT |
| M34552M8H-XXXFP | M4552M8H.DAT |
| M34552G8HFP | as above |
| M34553M8H-XXXFP | M4553M8H.DAT |
| M34553G8HFP | as above |
| M34556M8H-XXXFP | M4556M8H.DAT |
| M34556G8HFP | as above |
- How to Get and Set Up the MCU Data Files
| (1) | Download the compressed file "4552H.zip" (7.99 KB) of the MCU data files. |
| (2) | Decompress the downloaded file to obtain the 4552H folder. |
| (3) | Copy all the files, *.DATs and M34552.DBG, within the 4552H folder to the folder where the PD45M.EXE file resides. The old M34552.DBG file is overwritten with the new one.
Be sure to copy the M34552.DBG file and the *.DAT files at the same time. |
- Future Schedule
We plan to make the above MCU data files contained in the M3T-PD45M in its next and later upgrades.
|
 |