|
|
 |
RENESAS TOOL NEWS on December 16, 2003: RSO-HEW_1-031216D
Integrated Development Environment High-performance Embedded Workshop Upgraded to V.3.0.02
|
We have upgraded the High-performance Embedded Workshop, an integrated development environment, from Ver.3.01 to Ver.3.0.02.
Please refer to this release information together.
- Product and Version Concerned
- The High-performance Embedded Workshop Version 3.01 (release 1)
bundled with the M3T-NC30WA V.5.20 Release 1 C compiler
- The High-performance Embedded Workshop Version 3.01 (release 1)
bundled with the M3T-NC30WA C compiler (Free version for R8C/Tiny only)
- NOTE:
- If you want to use the High-performance Embedded Workshop with other compilers, refer to information about the High-performance Embedded Workshop Version 3.0.02.
- Descriptions of Upgrade
- 2.1 Specification Changed
- The category "C++ Class" in the navigation function is set to OFF by default.
- 2.2 Problem Fixed
- The known problem on the navigation function has been fixed.
For details, see RENESAS TOOL NEWS "A Note on Using Integrated Development Environment High-performance Embedded Workshop (On the Navigation Function)" issued on November 1, 2003.
- How to Get and Install the Upgraded Product
| (1) |
Please download the hewv3002u2.exe file from HERE.
|
| (2) | Then execute this file to complete the installation. |
- Notices
|
 |