|
|
 |
RENESAS TOOL NEWS on December 16, 2003: RSO-M3T-PD308SIM-031216D
A Note on Using Debuggers
M3T-PD308SIM, M3T-PD308F, M3T-PD308, and M3T-PD308M
|
Please take note of the following problem in using simulator debuggers and
emulator debuggers for the M32C/80 and M16C/80 series MCUs:
- On reverse-assemble display of the SCCnd instruction
- Products and Versions Concerned
Simulator debuggers:
M3T-PD308SIM V.1.00 Release 1 through V.3.10 Release 1
Emulator debuggers for the PC7501 emulator system:
All the versions of M3T-PD308F
Emulator debuggers for the PC4701 emulator system:
All the versions of M3T-PD308
Emulator debugger for compact emulators:
All the versions of M3T-PD308M
- Description
When the destination of an SCCnd instruction is register A0 or A1,
the reverse-assemble display of the instruction may show "???"
in the Program window and others.
Example in assembly language
-------------------------
SCNE A0
-------------------------
Example in reverse-assemble display
-------------------------
???
-------------------------
- Workaround
- 3.1 In the M3T-PD308SIM
- This problem has been fixed in the M3T-PD308SIM V.3.20 Release 1.
So, use this or later version of the product.
- 3.2 In the M3T-PD308F and M3T-PD308
- We supply the problem-fixed DLL file for each product. So, please
replace the DLL file in your product with the above-mentioned one
as follows:
| (1) |
Download the problem-fixed DLL file (compressed) you want.
p308fedll.exe for the M3T-PD308F (475KB)
p308edll.exe for the M3T-PD308 (469KB)
|
| (2) |
Decompress the downloaded file to obtain either of the following files:
p308fedll.dll (V.1.41.00) for the M3T-PD308F
p308edll.dll (V.1.41.00) for the M3T-PD308
|
| (3) |
With the decompressed file, overwrite the old file with the same
name in the folder where the product has been installed.
|
| (4) |
Confirm the version of the new DLL file as follows:
| (a) |
Launch your debugger.
|
| (b) |
Open the Help menu and select the About command. The
Version dialog box appears.
|
| (c) |
On this dialog box, confirm the version of the new file is
what you want.
|
|
- 3.3 In the M3T-PD308M
- We supply the problem-fixed DLL file for the product. So, please
replace the DLL file in your product with the above-mentioned one
as follows:
| (1) |
Download the problem-fixed p308mdll.exe file (compressed: 226KB)
|
| (2) |
Decompress the downloaded file to obtain the pdbdll.dll file (V.1.11.00).
|
| (3) |
With the decompressed file, overwrite the old file with the same
name in the folder where the product has been installed.
|
| (4) |
Confirm the DLL file has been updated as follows:
| (a) |
Launch your debugger. |
| (b) |
Open the Option menu and select the Line Assemble command.
The Line Assemble dialog box appears.
|
| (c) |
Type an SCCnd instruction "SCNE A0" in the Code edit box to
line-assemble and check whether the results of execution
are correctly displayed in the Line Assemble dialog box
and the Program window.
|
|
- Schedule of Fixing the Problem
We plan to fix this program in our next release of the M3T-PD308F,
M3T-PD308, and M3T-PD308M products.
|
 |