|
|
 |
RENESAS TOOL NEWS on March 16, 2004: RSO-M3T-NC308WA-040316D
C Compiler M3T-NC308WA Upgraded to V.5.20 Release 1
|
We have upgraded the M3T-NC308WA C-compiler (with an assembler and integrated development environment)
for the M32C/80 and M16C/80 series MCUs from V.5.10 Release 1 to V.5.20 Release 1.
- Descriptions of Upgrade
- 1.1 Functions Introduced
-
| (1) |
The High-performance Embedded Workshop supported. |
| (2) |
The following ten command options have been added:
| * | -fno_switch_table (-fNST)--Suppresses generation of code using a table jump for a switch statement |
| * | -fswitch_other_section (-fSOS)--Puts table code for a switch statement in a section other than the program section. |
| * | -fmake_vector_table (-fMVT)--Generates variable vector tables automatically. |
| * | -fmake_special_table (-fMST)--Generates special page tables automatically. |
| * | -Oforward_function_to_inline (-OFFTI)--Performs inline expansion for all the inline functions. |
| * | -Ofloat_to_inline (-OFTI)--Performs inline expansion of the run-time routine for executing floating-point operations to enhance the performance of these operations. |
| * | -Oglb_jmp (-OGJ)--Selects the most appropriate jump instruction at linking. |
| * | -Wno_used_function (-WNUF)--Outputs a warning message when a function not yet used in the application program is detected. |
| * | -Wstop_at_link (-WSAL)--Suppresses creation of absolute module files when a warning message is output at linking. |
| * | -Wundefined_macro (-WUM)--Outputs a warning message when a symbol not yet defined as a macro is used in a #if statement. |
|
| (3) |
Option /E, which enables multiple interrupts, has been added to expanded function #pragma INTHANDLER (#pragma HANDLER). |
- 1.2 Problems Fixed
- The following known problems have been fixed:
| (1) |
On the "MOVA" and "PUSHA" mnemonic instructions For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers and Assemblers M3T-NC308WA, M3T-NC30WA, AS308, and AS30"issued on May 1, 2003. |
| (2) |
On standard library functions atof and strtod For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA, M3T-NC30WA, M3T-NC79WA and M3T-NC77WA" issued on May 16, 2003. |
| (3) |
On arithmetic right shift of a variable of type long long For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC308WA" issued on June 1, 2003. |
| (4) |
On defining structure-type arrays For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA, M3T-NC30WA, M3T-NC79WA, and M3T-NC77WA" issued on June 1, 2003. |
| (5) |
On displaying the values of arguments passed to a function For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on June 16, 2003. |
| (6) |
On using the -Ocompare_byte_to_word (-OCBTW) compile option |
| (7) |
On the character string length of a variable that has functions as array elements For details of (6) and (7), see
RENESAS TOOL NEWS "Notes on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on July 16, 2003. |
| (8) |
On arguments of formatted input/output functions For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA, M3T-NC30WA, M3T-NC79WA, and M3T-NC77WA" issued on August 16, 2003. |
| (9) |
On calling a function indirectly For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC308WA" issued on August 16, 2003. |
| (10) |
On using the link option "-U" For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on September 16, 2003. |
| (11) |
On comparing a variable with another one or a constant of type signed char in a conditional expression For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC308WA" issued on October 16, 2003. |
| (12) |
On the division and remainder operations between constants For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on October 16, 2003. |
| (13) |
On linking relocatable module files with no sections For details, see
RENESAS TOOL NEWS "A Note on Using C compilers M3T-NC308WA, M3T-NC30WA, and M3T-NC79WA; and Assemblers AS308, AS30, and AS79 --On Linking Relocatable Files--" issued on November 16, 2003. |
| (14) |
On declaring parameters in function definitions For details, see
RENESAS TOOL NEWS "A Note on Using C compilers M3T-NC308WA and M3T-NC30WA --On Declaring Parameters in Function Definitions--" issued on November 16, 2003. |
| (15) |
On function calls using the indirection operator For details, see
RENESAS TOOL NEWS "A Note on Using C compilers M3T-NC308WA and M3T-NC30WA --On Function Calls Using the Indirection Operator--" issued on November 16, 2003. |
| (16) |
On defining array-type variables For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on January 16, 2004. |
| (17) |
On casting an integer-type value to a pointer-type one For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC308WA" issued on January 16, 2004. |
| (18) |
On testing equality/inequality between a variable of type signed or unsigned char and a constant For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA --On Testing Equality/Inequality Between a Variable and a Constant--" issued on March 1, 2004. |
- How to Upgrade the Current Product and Order the Upgraded One
- 2.1 Online Upgrade (without Charge)
- Please download the upgraded product from HERE.
- 2.2 First ordering or upgrading by CD-ROM (with Additional Charge)
- Upgrade service in CD-ROM is also available. When you place an order, please furnish the following information to your local Renesas Technology sales office or distributor:
First Ordering
| Product Type | : | M3T-NC308WA |
| Version No. | : | V.5.20 |
| Release No. | : | Release 1 |
| Host OS | : | Windows XP, Windows Me, Windows 98, Windows 2000, or Windows NT 4.0 |
Upgrading by CD-ROM
Please let us know your product's license ID or serial number besides the above information.
|
 |