|
|
 |
RENESAS TOOL NEWS on March 16, 2004: RSO-M3T-NC30WA-040316D
C Compiler M3T-NC30WA Upgraded to V.5.30 Release 1
|
We have upgraded the M3T-NC30WA C-compiler (with an assembler and integrated development environment)
for the M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, and R8C/Tiny series MCUs from V.5.20 Release 1 to V.5.30 Release 1.
- Descriptions of Upgrade
- 1.1 Functions Introduced
-
| (1) |
The following eight command options have been added:
| * | -fno_switch_table (-fNST)--Suppresses generation of code using a table jump for a switch statement |
| * | -fmake_vector_table (-fMVT)--Generates variable vector tables automatically. |
| * | -fmake_special_table (-fMST)--Generates special page tables automatically. |
| * | -Oforward_function_to_inline (-OFFTI)--Performs inline expansion for all the inline functions. |
| * | -Wno_used_function (-WNUF)--Outputs a warning message when a function not yet used in the application program is detected. |
| * | -Wstop_at_link (-WSAL)--Suppresses creation of absolute module files when a warning message is output at linking. |
| * | -Wundefined_macro (-WUM)--Outputs a warning message when a symbol not yet defined as a macro is used in a #if statement. |
| * | -Oglb_jmp (-OGJ)--Selects the most appropriate jump instruction according to the jump distance at linking |
|
| (2) |
Option /E, which enables multiple interrupts, has been added to expanded function #pragma INTHANDLER (#pragma HANDLER). |
- 1.2 Problems Fixed
- The following known problems have been fixed:
| (1) | On using the link option "-U" For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on September 16, 2003. |
| (2) | On using the standard library function "strcpy" For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC30WA V.5.20 Release 1" issued on October 1, 2003. |
| (3) | On the division and remainder operations between constants For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on October 16, 2003. |
| (4) | On using the enhancing patch tool of the Scan All Dependencies function |
| (5) | On using the Options dialog box For details of (4) and (5), see
RENESAS TOOL NEWS "Notes on Using C Compiler M3T-NC30WA V.5.20 Release 1" issued on October 16, 2003. |
| (6) | On linking relocatable module files with no sections For details, see
RENESAS TOOL NEWS "A Note on Using C compilers M3T-NC308WA, M3T-NC30WA, and M3T-NC79WA; and Assemblers AS308, AS30, and AS79 --On Linking Relocatable Files--" issued on November 16, 2003. |
| (7) | On declaring parameters in function definitions For details, see
RENESAS TOOL NEWS "A Note on Using C compilers M3T-NC308WA and M3T-NC30WA --On Declaring Parameters in Function Definitions--" issued on November 16, 2003. |
| (8) | On function calls using the indirection operator For details, see
RENESAS TOOL NEWS "A Note on Using C compilers M3T-NC308WA and M3T-NC30WA --On Function Calls Using the Indirection Operator--" issued on November 16, 2003. |
| (9) | On defining array-type variables For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on January 16, 2004. |
| (10) | On referencing members in a union For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA --On Referencing Members in a Union--" issued on March 1, 2004. |
| (11) | On using standard library function "strcpy" For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC30WA --On Using Standard Library Function "strcpy"--" issued on March 1, 2004. |
| (12) | On an OR operation between a variable and a constant For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC30WA --On an OR Operation Between a Variable and a Constant--" issued on March 1, 2004. |
- How to Upgrade the Current Product and Order the Upgraded One
- 2.1 Online Upgrade (without Charge)
- Please download the upgraded product from HERE.
- 2.2 First ordering or upgrading by CD-ROM (with Additional Charge)
- Upgrade service in CD-ROM is also available. When you place an order, please furnish the following information to your local Renesas Technology sales office or distributor:
First Ordering
| Product Type | : | M3T-NC30WA |
| Version No. | : | V.5.30 |
| Release No. | : | Release 1 |
| Host OS | : | Windows XP, Windows Me, Windows 98, Windows 2000, or Windows NT 4.0 |
Upgrading by CD-ROM
Please let us know your product's license ID or serial number besides the above information.
|
 |