|
|
 |
RENESAS TOOL NEWS on April 1, 2004: RSO-M3T-NC8C-040401D
R8C/Tiny-only Free-version Compiler M3T-NC8C
Upgraded to V.5.30 Release 1
|
We have upgraded the R8C/Tiny-only Free-version Compiler M3T-NC8C from M3T-NC30WA V.5.20 Release 1 to V.5.30 Release 1.
NOTE:
The product name of R8C/Tiny-only Free-version Compiler has been changed
from M3T-NC30WA to M3T-NC8C on and after April 1, 2004.
R8C/Tiny-only free-version compiler M3T-NC8C was integrated into the evaluation version of C compiler package M3T-NC30WA for M16C series.
- Descriptions of Upgrade
- 1.1 Functions Introduced
-
| (1) |
The following eight command options have been added:
| * | -fno_switch_table (-fNST)--Suppresses generation of code using a table jump for a switch statement |
| * | -fmake_vector_table (-fMVT)--Generates variable vector tables automatically. |
| * | -Oforward_function_to_inline (-OFFTI)--Performs inline expansion for all the inline functions. |
| * | -Wno_used_function (-WNUF)--Outputs a warning message when a function not yet used in the application program is detected. |
| * | -Wstop_at_link (-WSAL)--Suppresses creation of absolute module files when a warning message is output at linking. |
| * | -Wundefined_macro (-WUM)--Outputs a warning message when a symbol not yet defined as a macro is used in a #if statement. |
| * | -Oglb_jmp (-OGJ)--Selects the most appropriate jump instruction according to the jump distance at linking |
|
| (2) |
Option /E, which enables multiple interrupts, has been added to expanded function #pragma INTHANDLER (#pragma HANDLER). |
- 1.2 Problems of Compiler Fixed
- The following known problems have been fixed:
| (1) | On using the link option "-U" For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on September 16, 2003. |
| (2) | On using the standard library function "strcpy" For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC30WA V.5.20 Release 1" issued on October 1, 2003. |
| (3) | On the division and remainder operations between constants For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on October 16, 2003. |
| (4) | On using the enhancing patch tool of the Scan All Dependencies function |
| (5) | On using the Options dialog box For details of (4) and (5), see
RENESAS TOOL NEWS "Notes on Using C Compiler M3T-NC30WA V.5.20 Release 1" issued on October 16, 2003. |
| (6) | On linking relocatable module files with no sections For details, see
RENESAS TOOL NEWS "A Note on Using C compilers M3T-NC308WA, M3T-NC30WA, and M3T-NC79WA; and Assemblers AS308, AS30, and AS79 --On Linking Relocatable Files--" issued on November 16, 2003. |
| (7) | On declaring parameters in function definitions For details, see
RENESAS TOOL NEWS "A Note on Using C compilers M3T-NC308WA and M3T-NC30WA --On Declaring Parameters in Function Definitions--" issued on November 16, 2003. |
| (8) | On function calls using the indirection operator For details, see
RENESAS TOOL NEWS "A Note on Using C compilers M3T-NC308WA and M3T-NC30WA --On Function Calls Using the Indirection Operator--" issued on November 16, 2003. |
| (9) | On defining array-type variables For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA" issued on January 16, 2004. |
| (10) | On referencing members in a union For details, see
RENESAS TOOL NEWS "A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA --On Referencing Members in a Union--" issued on March 1, 2004. |
| (11) | On using standard library function "strcpy" For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC30WA --On Using Standard Library Function "strcpy"--" issued on March 1, 2004. |
| (12) | On an OR operation between a variable and a constant For details, see
RENESAS TOOL NEWS "A Note on Using C Compiler M3T-NC30WA --On an OR Operation Between a Variable and a Constant--" issued on March 1, 2004. |
- 1.3 Problems of Integrated Development Environment High-performance Embedded Workshop Fixed
- The following known problems have been fixed:
- How to Upgrade Your Product
Inform Tool Technical Support of the purpose of upgrading.
Tool Technical Support: csc@renesas.com
|
 |