Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on April 1, 2004: RSO-M3T-CC32R-040401D

Simulator Debuggers
Bundled with C Compilers and Assemblers
for the 8-, 16-, and 32-Bit MCUs

We notify you that we started supplying simulator debuggers bundled with C compilers and assemblers on this April 1.

  1. Descriptions
    • Our simulator debuggers, which have been sold separately from C compilers and assemblers for the 8-, 16-, and 32-bit MCUs, are bundled with each of them, as shown in the table below.
    • The simulator debuggers to be bundled, which were upgraded and released on this April 1, can be installed using the license ID of C compilers and assemblers.
    • These simulator debuggers are provided free of charge for the customers who are using any of the compilers and assemblers concerned.


  2. Versions of Simulator Debuggers Bundled
    The current simulator debuggers concerned were upgraded to the versions listed below on April 1.
    For details, see "Simulator Debuggers M3T-PD32RSIM, M3T-PD308SIM, M3T-PD30SIM, M3T-PD79SIM, M3T-PD77SIM, and M3T-PD38SIM Upgraded" issued on April 1, 2004, in this series of news.

    C Compiler or Assembler Simulator Debugger
    M3T-CC32R Cross-tool kit
    for M32R family
    M3T-PD32RSIM V.2.10 Release 1A
    M3T-NC308WA C compiler
    for M32C/80 and M16C/80 series
    M3T-PD308SIM V.3.20 Release 1A
    M3T-NC30WA C compiler
    for M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, and R8C/Tiny series
    M3T-PD30SIM V.5.20 Release 1A
    M3T-NC79WA C compiler
    for 79xx series
    M3T-PD79SIM V.3.20 Release 1A
    M3T-NC77WA C compiler
    for 77xx series
    M3T-PD77SIM V.3.10 Release 1A
    M3T-RASM77Relocatable assembler
    for 77xx series
    M3T-PD77SIM V.3.10 Release 1A
    M3T-SRA74Relocatable assembler
    for 740 family
    M3T-PD38SIM V.2.10 Release 1A


  3. First Shipping of Bundled Products
    On April 1, 2004.


  4. How to Get C compilers, Assemblers, and Simulator Debuggers after April 1

    (1) If you need a C compiler, an assembler, and a simulator debugger, place an order for the C compiler and assembler only. And we will ship their latest versions in CD-ROM with the corresponding simulator debugger bundled.

    (2) If you have been using a Renesas-made C compiler and assembler and need a simulator debugger only, download the simulator debugger free of charge from HERE.
    The downloaded simulator debugger can be installed using your C compiler and assembler's license ID.

    (3) If you have been using a partner-made C compiler and assembler and need a simulator debugger only, place an order for the simulator debugger as before. And we will ship its latest version in CD-ROM. Please furnish the following information on it to your local Renesas Technology sales office or distributor:

    Product Type
    Version No.
    Release No.
    CommentWIN

    Note, however, that though this CD-ROM contains a C compiler, an assembler, and a simulator debugger, it comes with the license ID for installing only the simulator debugger.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal