Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on April 1, 2004: RSO-M3T-PD32RSIM-040401D

Simulator Debuggers
M3T-PD32RSIM, M3T-PD308SIM, M3T-PD30SIM,
M3T-PD79SIM, M3T-PD77SIM, and M3T-PD38SIM
Upgraded

We have upgraded our simulator debuggers to the following versions:
  • M3T-PD32RSIM V.2.10 Release 1A for the M32R family
  • M3T-PD308SIM V.3.20 Release 1A for the M32C/80 and M16C/80 series
  • M3T-PD30SIM V.5.20 Release 1A for the M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, and R8C/Tiny series
  • M3T-PD79SIM V.3.20 Release 1A for the 79xx series
  • M3T-PD77SIM V.3.10 Release 1A for the 77xx series
  • M3T-PD38SIM V.2.10 Release 1A for the 740 family


  1. Summary
    We started supplying simulator debuggers bundled with C compilers and assemblers for the 8-, 16-, and 32-bit MCUs on this April 1. According to this change of shipment, we upgraded these simulator debuggers.
    For details of bundling, see RENESAS TOOL NEWS "Simulator Debuggers Bundled with C Compilers and Assemblers for the 8-, 16-, and 32-Bit MCUs" issued on April 1, 2004, in this series of news.

  2. Description
    Each of the upgraded simulator debuggers, subject to no changes of its functions, can be installed using the license ID of the corresponding C compiler and assembler.
    Note, however, that our C compilers and assemblers cannot be installed using the license ID of any simulator debugger.


  3. Online Upgrade (Without Charge)
    Please download the upgraded product you want from HERE.


  4. First ordering
    If you have been using a partner-made C compiler and assembler and place an order for a Renesas-made simulator debugger only, please furnish the following information on it to your local Renesas Technology sales office or distributor:

    Product Type
    Version No.
    Release No.
    CommentWIN

    Note, however, that though this CD-ROM contains a C compiler, an assembler, and a simulator debugger, it comes with the license ID for installing only the simulator debugger.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal