|
|
 |
RENESAS TOOL NEWS on April 1, 2004: RSO-M3T-PD308F-040401D
Emulator Debuggers M3T-PD308F, M3T-PD30F, M3T-PD308, M3T-PD30, M3T-PD79, M3T-PD77, and M3T-PD38 Upgraded
|
We have upgraded the emulator debuggers used in combination with the PC7501 and PC4701 emulators to the following versions:
- Emulator Debuggers Used in the PC7501 emulator
M3T-PD308F V.3.20 Release 1 for the M32C/80 series
M3T-PD30F V.2.20 Release 1 for the M16C/60 and M16C/Tiny series
- Emulator Debuggers Used in the PC4701 emulator
M3T-PD308 V.5.20 Release 1 for the M32C/80,and M16C/80 series
M3T-PD30 V.8.20 Release 1 for the M16C/60, /30, /Tiny, /20, /10 series
M3T-PD79 V.4.20 Release 1 for the 79xx series
M3T-PD77 V.4.20 Release 1 for the 77xx series
M3T-PD38 V.5.20 Release 1 for the 740 family
- Summary
We started supplying the M3T-PD308F and M3T-PD30F emulator debuggers bundled with the PC7501 emulator for the M16C family MCUs on this April 1.
We also provide the customers who own or are renting the PC4701 emulator with its emulator debuggers free of charge.
According to this change of shipment, we upgraded the above emulator debuggers.
For details of bundling, see the following items of RENESAS TOOL NEWS:
both issued on April 1, 2004 in this series of news.
- Descriptions of Upgrade
- 2.1 New Features
-
| (1) | All the emulator debuggers concerned can be installed without any
license ID. |
| (2) | The M16C/Tiny series MCUs are supported (in the M3T-PD30F only). |
- 2.2 Problems Fixed
-
| (1) | In the MR trace and MR analyze Windows,
the display of history of OS-independent interrupts and of the tasks and interrupts affected by the generation
of OS-independent interrupts are incorrect (in the M3T-PD308F only). |
| (2) | All the breakpoints and address match interrupt breakpoints
that have been previously set are deleted at downloading the target program
(in the M3T-PD308F, M3T-PD30F, M3T-PD308, and M3T-PD30). |
- 2.3 Problems Fixed
- The following problems have been fixed:
- Online Upgrade (Without Charge)
Please download the upgraded product you want from HERE.
|
 |