|
|
 |
RENESAS TOOL NEWS on May 1, 2004: RSO-M3T-MR32R-040501D
Corrections to the Reference Manuals
of Real-Time OSes M3T-MR32R
|
We notify corrections to the reference manuals of the M3T-MR32R real-time OSes for the M32R family MCUs as stated below.
- Documents Concerned
The reference manuals included with the M3T-MR32R V.3.00 Release 1 through V.3.50 Release 2
- Corrections
| (1) |
Section 2.11.2, "ref_sys(Refer System Status)"
In the TSS_LOC row of the Value column in the sysstat table, read 3 for 2 |
| (2) |
Section 3.6, "Common Constants and Packet Format of Structure"
For the statements from the beginning of the typedef struct t_regs definition
up to the end of the typedef struct t_exc one (before the comment
"Related to Implementation-Dependent System Call (Mailbox)," read as follows:
/* Register Information Packets
when forced exception has occurred */
typedef struct t_regs {
VW r0; /* Contents of R0 register at that time */
VW r1; /* Contents of R1 register at that time */
VW r2; /* Contents of R2 register at that time */
VW r3; /* Contents of R3 register at that time */
VW r4; /* Contents of R4 register at that time */
VW r5; /* Contents of R5 register at that time */
VW r6; /* Contents of R6 register at that time */
VW r7; /* Contents of R7 register at that time */
VW r8; /* Contents of R8 register at that time */
VW r9; /* Contents of R9 register at that time */
VW r10; /* Contents of R10 register at that time */
VW r11; /* Contents of R11 register at that time */
VW r12; /* Contents of R12 register at that time */
VW r13; /* Contents of R13 register at that time */
VW r14; /* Contents of R14 register at that time */
VW sp; /* Contents of SP register at that time */
VW accl; /* Contents of ACCL register at that time */
VW acch; /* Contents of ACCH register at that time */
VW acc1l; /* Contents of ACC1L register at that time
(the value of FPSR when kernel for FPU used;
indefinite except when kernels for FPU
and M32Rx/D used) */
VW acc1h; /* Contents of ACC1H register at that time
(indefinite except when kernel for M32Rx/D used) */
} T_REGS;
/* EIT Information Packets */
typedef struct t_reit {
PSW psw; /* Contents of PSW register at that time */
FP pc; /* Contents of PC at that time */
} T_EIT;
/* Exception Information Packets */
typedef struct t_exc {
W exckind; /* kind of exception: always set to EXK_TER=2
(forced exception) */
UW exccd; /* exception code */
ID tskid; /* task ID */
UW exeenv; /* system status where exception has occurred:
always set to TTE_TSK=0
(task is under execution) */
} T_EXC;
|
|
 |