Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on May 1, 2004: RSO-E7_2-040501D

A Note on Using
the Tiny/SLP E7 Emulator Software

--On Downloading a Firmware File to the Data Flash Area--

Please take note of the following problem in using the Tiny/SLP E7 Emulator Software:
  • On downloading a firmware file to the data flash area


  1. Versions Concerned
    Tiny/SLP E7 Emulator Software V.2.3.01 and later


  2. Description
    Assume that a firmware file has been downloaded to the data flash area of the R5F21124 MCU belonging to the R8C/12 group or the R5F21134 to the R8C/13, and then the High-performance Embedded Workshop, an integrated development environment, has been launched. Under such conditions, clearing the Data Area Access Enable bit PM10 (bit 0 of address 05h) to 0 (that is, disabled) during executing or debugging the user program causes a timeout error to arise.


  3. Workaround
    If a firmware file is downloaded to the data flash area, don't clear PM10 to 0.


  4. Schedule of Fixing the Problem
    Sorry that this problem is unavoidable in the Tiny/SLP E7 Emulator Software.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal