|
|
 |
RENESAS TOOL NEWS on May 16, 2004: RSO-M3T-PD32RM-040516D
Emulator Debuggers M3T-PD32RM and M3T-PD32R Upgraded
|
We have upgraded the emulator debuggers for the M32R family MCUs as follows:
- M3T-PD32RM for the M32100T5-SDI-E, M32100T3-SDI-E and M32100T-EZ-E emulators:
from V.2.00 Release 1 to V.2.10 Release 1
- M3T-PD32R for the M32100T2-SDI-E emulator:
from V.4.00 Release 1 to V.4.10 Release 1(*)
NOTE:
| (*) |
Also supports the following emulators used for repair and spare only:
M32120T-SDI, M32120T-SDI, M32100T-SDI-E,
M32170T-SDI, M32310T-SDI-E, and M32310T-SDI |
- Descriptions of Upgrade
- 1.1 Functions Introduced
-
| (1) | The M32100T5-SDI-E emulator supported (in M3T-PD32RM only). |
| (2) | The Data Trace window introduced (in M3T-PD32RM only): it analyzes
the results of real-time trace measurement and graphically displays
information on data accesses (reads from and writes to memory). |
| (3) | The AddPath script command added: it gives the search path (directory
path name) to the directory where source files are searched for. |
- 1.2 Functions Improved
-
| (1) |
In the Trace window
| (a) |
Two or more display modes are selectable. When disassemble
and source modes of displays are selected, the results of
disassemble are displayed immediately after the source lines. |
| (b) |
The results of trace measurement are displayed and identified
by color; for example, red and blue represent trace data
showing reads from and writes to memory respectively. |
| (c) |
Time information of trace measurement results can be displayed
using one mode selected from the following three:
| * Absolute Time: |
Elapsed time from the beginning of program execution to each measurement time |
| * Difference: |
Differential time between each measurement time and its immediately preceding one. |
| * Relative time: |
Relative time between a selected piece of
trace data and another (a selected piece
of trace data is displayed in Absolute Time). |
|
|
| (2) |
In the MR window
In addition to the statuses of OS resources such as tasks,
mailboxes, and semaphores, those of message buffers, ports and
prioritized mailboxes can also be displayed.
Furthermore, the statuses of OS resources, which can hitherto
be displayed only during the halt of the target system, is now
seen during the execution of the target.
|
- 1.3 Problems Fixed
- The following known problems have been fixed:
- How to Upgrade the Current Products
- 2.1 Online Upgrade (without Charge)
- Please download the upgraded product you want from HERE.
|
 |