Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on May 16, 2004: RSO-M3T-NC308WA-040516D

A Note on Using C-Compiler Packages
M3T-NC308WA and M3T-NC30WA
--On Debug Information--

Please take note of the following problem in using the M3T-NC308WA and M3T-NC30WA C-compiler packages (with assembler and integrated development environment):
  • On debug information


  1. Products and Versions Concerned
    M3T-NC308WA V.1.00 Release 1 through V.5.20 Release 1
      for the M32C/80, and M16C/80 series MCUs
    M3T-NC30WA V.1.00 Release 1 through V.5.30 Release 1
      for the M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, and R8C/Tiny series MCUs


  2. Description
    Breakpoints may not be set in the functions defined within the files included by the #include preprocess command.


  3. Workaround
    Define functions in a C source file.


  4. Schedule of Fixing the Problem
    We plan to fix this problem in our next release of the products.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal