Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on June 16, 2004: RSO-HEW-040616D

A Note on Using
Integrated Development Environment High-performance Embedded Workshop

Please take note of the following problem in using the High-performance Embedded Workshop, an integrated development environment:
  • On using the Import Makefile function


  1. Products Concerned
    The High-performance Embedded Workshops included with the following products
    (1) C compiler package for the M32R family MCUs
         M3T-CC32R V.4.20 Release 1
    (2) C compiler package for the M32C/80, and M16C/80 series MCUs
         M3T-NC308WA V.5.20 Release 1
    (3) C compiler packages for the M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, and R8C/Tiny series MCUs
         M3T-NC30WA V.5.20 Release 1 and V.5.30 Release 1
    (4) Freeware product specific to the R8C/Tiny series
         M3T-NC30WA V.5.20 Release 1(*)
         M3T-NC8C V.5.30 Release 1

    NOTE:
    * This product's name was changed from M3T-NC30WA to M3T-NC8C on April 1, 2004.


  2. Description
    When reading an already-existing makefile and creating a project by going through the following steps, some items of information on options become unavailable.

    (1)The Import makefile selected in the project list of the New Project Workspace dialog box; then the OK button clicked. The New Project-1/4-Import Makefile wizard will appear.
    (2)The button with the picture of a folder clicked; then the Import Makefile dialog box will appear.
    (3)A file clicked in the file list; then the OK button clicked. The file name set the Makefile path: text box. The Import options check box checked and the Next > button or the Finish button clicked.


  3. Workaround
    Don't check the Import options check box in the New Project-1/4-Import Makefile wizard. Instead, the options must be set as follows:
    (1) After creating a project, open the Options menu on the menu bar and select the Renesas Mxxx(*) Standard Toolchain command.
    (2) You see the Renesas Mxxx(*) Standard Toolchain dialog box opens. In this dialog box, set the Import options.

    NOTE:
    * Mxxx denotes the family name of the tool chain you are using.


  4. Schedule of Fixing the Problem
    We plan to include the problem-fixed High-performance Embedded Workshop with each of the C compiler packages concerned in our next release of those.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal