Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on July 1, 2004: RSO-M34519T-MCU-040701D

Corrections to the M34519T-MCU User's Manual

We notify the corrections to the user's manual of the M34519T-MCU board for the 4518, 4519, 4583, and 4584 groups in the 4500 series MCUs. The document number concerned is REJ10J0071-0100Z.

  1. Descriptions
    In Figures 5.1 and 5.2 in Chapter 5 "Connection Circuit Diagrams", there are found errors in the connector-pin-hole numbers connected to the target system (in J3-16B, for example, J3 represents a connector number and 16B a pin-hole one). The corrections are shown below.

    1.1 Page 29, the top right portion of Figure 5.1
    Read the connector-pin-hole number in the second column for the one in the third column for each signal name as follows:

     Signal NameConnector-Pin-Hole No.
    Read For
    1.D6/CNTR0J3-8C J3-16B
    2.D7/CNTR1J3-9C J3-15B
    3.P50 J3-10CJ3-14B
    4.P51 J3-11CJ3-13B
    5.P52 J3-12CJ3-12B
    6.P53 J3-13CJ3-11B
    7.P30/INT0J3-19DJ3-10B
    8.P31/INT1J3-18DJ3-9B
    9.P32 J3-17DJ3-8B
    10.P33 J3-16DJ3-7B
    11.P60/AIN0J3-15DJ3-6B
    12.P61/AIN1J3-14DJ3-5B
    13.P62/AIN2J3-13DJ3-4B
    14.P63/AIN3J3-12DJ3-3B
    15.P40/AIN4J3-11DJ3-2B
    16.P41/AIN5J3-10DJ3-1B
    17.P42/AIN6J3-9D J3-1A
    18.P43/AIN7J3-8D J3-2A
    19.ERESET* J3-17CJ4-5A

    1.2 Page 30, the top right portion of Figure 5.2
    Read the connector-pin-hole number in the second column for the one in the third column for each signal name as follows:

     Signal NameConnector-Pin-Hole No.
    Read For
    1.EP00 J3- 7DJ4- 5B
    2.EP01 J3- 6DJ4- 6B
    3.EP02 J3- 5DJ4- 7B
    4.EP03 J3- 4DJ4- 8B
    5.EP10 J3- 3DJ4- 9B
    6.EP11 J3- 2DJ4-10B
    7.EP12 J3- 1DJ4-11B
    8.EP13 J3- 1CJ4-12B
    9.ED0 J3- 2CJ4-13B
    10.ED1 J3- 3CJ4-14B
    11.ED2 J3- 4CJ4-15B
    12.ED3 J3- 5CJ4-16B
    13.ED4 J3- 6CJ4-16A
    14.ED5 J3- 7CJ4-15A



  2. How to Get the Corrected User's Manual of the M34519T-MCU
    The document number of the corrected manual has been changed to REJ10J0071-0200Z. Please download this manual from HERE. The document, written in PDF, is 36 pages in length and 288 KB in size.
    This PDF manual is due to be released also on our tool homepage in the end of July, 2004.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal