|
|
 |
RENESAS TOOL NEWS on July 1, 2004: RSO-M34282T2-CPE-040701D
Compact Emulator M34282T2-CPE
for the 4282 Group of the 720 Series MCUs Released
|
We have released the M34282T2-CPE compact emulator for the 4282 group of
the 720 series in the 720 family MCUs.
- Outline
The M34282T2-CPE is a compact emulator for the 4282 group of the 720
series MCUs, provided with real-time trace and hardware-break functions.
Its features are as follows:
- Debugging functions more enhanced than the PC4400 system (equivalent to the PC4504 system in basic debugging functions)
- Real-time trace function supported
- Smaller than the PC4400 system in size
- Programming and debugging tools included
- Economical price
- USB (USB1.1 full-speed) supported
- The Contents of the Product Package
| (1) | An emulator--M34282T2-CPE |
| (2) | An evaluation MCU--M34282E2GP (already mounted) |
| (3) | A USB interface cable (1.8 m) |
| (4) | A power cable (30 cm; no power supply included) |
| (5) | An external trace cable |
| (6) | A 20-conductor standard-pitch cable |
| (7) | Three oscillator boards
- OSC-2 for 4-MHz main clock (already mounted)
- OSC-2 for 500-kHz main clock
- Bare board for OSC-2 (used for another frequency)
|
| (8) | An M3T-PD72M emulator debugger (specific to the compact emulator) and an ASM72 absolute assembler (both included with the product) |
| (9) | A user's manual in PDF |
For further information, see its datasheet.
- First Ordering
If you place an order for the product, please provide the following
items of information for your local Renesas Technology sales office
or distributor:
| Product Type | Type Name | Comment |
| M34282T2-CPE | M34282T2-CPE | -- |
|
 |