|
|
 |
RENESAS TOOL NEWS on September 1, 2004: RSO-M3T-PD32RM-040901D
A Note on Using Emulator Debuggers
M3T-PD32RM, M3T-PD32R, M3T-PD308F, M3T-PD308, M3T-PD30F and M3T-PD30
|
Please take note of the following problem in using the M3T-PD32RM, M3T-PD32R,
M3T-PD308F, M3T-PD308, M3T-PD30F, and M3T-PD30 emulator debuggers:
- On expanding a global variable in the C Watch window
- Products and Versions Concerned
M3T-PD32RM V.2.00 Release 1 and V.2.10 Release 1
(for the M32100T5-SDI-E, M32100T3-SDI-E, and M32100T-EZ-E emulators)
M3T-PD32R V.4.00 Release 1 and V.4.10 Release 1
(for the M32100T2-SDI-E emulator)
M3T-PD308F V.3.00 Release 1 through V.3.20 Release 1
(for the M32C/80 series of MCUs)
M3T-PD308 V.5.00 Release 1 through V.5.20 Release 1
(for the M32C/80 and M16C/80 series of MCUs)
M3T-PD30F V.2.00 Release 1 through V.2.20 Release 1
(for the M16C/60, M16C/30 and M16C/Tiny series of MCUs)
M3T-PD30 V.8.00 Release 1 through V.8.20 Release 1
(for the M16C/60, /30, /Tiny, /20 and /10 series of MCUs)
- Description
In the C Watch window, expanding a global variable in a structure,
a union, or an array of structures or unions may cause the emulator
debugger to terminate unsuccessfully.
- 2.1 Conditions
- This problem occurs if you go through the following steps:
| (1) |
Select "On-Demand" as a saving mode of debug information;
then download the target program. |
| (2) |
In the C Watch window, display a global variable in a structure,
a union, or an array of structures or unions (without expanding it). |
| (3) |
Perform the function that switch file scopes from one to another;
for example, step execution and Set PC. Here in the file scope
after switching, no variable of the same type as the one in (2)
has been defined. |
| (4) |
Expand the variable in (2). |
- Workaround
This problem can be circumvented in either of the following ways:
| (1) |
Change the "On-Demand" mode to the "On-Memory" mode as a saving mode
of debug information. To do so, open the Init dialog box, click the
Debugging Information tab, and uncheck the On Demand check box. |
| (2) |
Use the problem-fixed DLL file. To do so, replace the DLL file
in your product with the problem-fixed one as follows:
| 1. |
Download the compressed problem-fixed DLL files.
|
| 2. |
Decompress the downloaded files. The names and versions of the decompressed files are as follows:
| File Name | Version No. | Used For |
| p32rmedll.dll | V.1.30.02 | M3T-PD32RM |
| p32redll.dll | V.1.30.01 | M3T-PD32R |
| p308fedll.dll | V.1.51.00 | M3T-PD308F |
| p308edll.dll | V.1.51.00 | M3T-PD308 |
| p30fdll.dll | V.1.31.00 | M3T-PD30F |
| p30edll.dll | V.1.51.00 | M3T-PD30 |
|
| 3. |
Copy the decompressed DLL file you want into the folder where
your emulator debugger resides. The current DLL file will be
overwritten with the new one. |
| 4. |
Check for the version of the DLL file as follows:
| (a) | Launch the emulator debugger. |
| (b) | Open the Help menu and select the About command. The Version dialog box appears. |
| (c) | In the dialog box, check to see that the version number displayed is that of the problem-fixed DLL file. |
|
|
- Schedule of Fixing the Problem
We plan to fix this problem in our next release of the products.
|
 |