|
|
 |
RENESAS TOOL NEWS on September 1, 2004: RSO-E7-040901D
|
A Note on Using E7 Emulator Software
|
Please take note of the following problem in using the E7 emulator software:
- On debugging the R8C/Tiny MCU series (except the 16-KB ROM version)
- Versions Concerned
E7 emulator software V.2.0.01, V.2.0.02, and V.2.1.00
- Description
At debugging any MCU in the R8C/Tiny series (except the 16-KB ROM version),
if the R5F21102, R5F21103, R5F21112, or R5F21113 is selected after
establishing the communication between the E7 emulator and the E7 emulator
software, the following problem occurs:
| |
After writes to the flash memory for downloading a user program have
started, a timeout error will arise in the High-performance Embedded Workshop, and the High-performance Embedded Workshop will
become unmanageable. |
- Solution
This problem has already been resolved in the E7 emulator software
V.2.3.01 or later. To update the E7 emulator software, please download
its update program from HERE.
|
 |