Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on October 16, 2004: RSO-HEW_1-041016D

A Note on Using
Integrated Development Environment High-performance Embedded Workshop
--On Using SQMlint Options--

Please take note of the following problem in using the High-performance Embedded Workshop, an integrated development environment:
  • On using SQMlint options in the MISRA C rule checker


  1. Products Concerned
    The High-performance Embedded Workshop included with the following product:
      M3T-CC32R V.4.30 Release 00 (C compiler package for the M32R family)


  2. Description
    If the High-performance Embedded Workshop is used in combination with the SQMlint, the following problem arises:
    In the High-performance Embedded Workshop, open the Options menu and select the Renesas M32R Standard Toolchain command. You see the Renesas M32R Standard Toolchain dialog box. However, the list of the SQMlint options is not provided in this dialog box.


  3. Workaround
    Select any SQMlint option as follows:
    (1)Open the Options menu and select Renesas M32R Standard Toolchain. The Renesas M32R Standard Toolchain dialog box appears.
    (2)Click the C tab in this dialog box.
    (3)Then select Other in the Category list. The User defines options text box appears.
    (4)Type the SQMlint option you want in this text box.
    (5)Click the OK button.


  4. Schedule of Fixing the Problem
    In our next release of the M3T-CC32R C compiler package, we plan to include the problem-fixed High-performance Embedded Workshop in it.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal