|
|
 |
RENESAS TOOL NEWS on October 16, 2004: RSO-SHC-041016D
A Note on Using a C/C++ Compiler V.9.00 Release 00 for the SuperH RISC engine Family CPUs
|
Please take note of the following problem in using a C/C++ compiler package
for the SuperH RISC engine family of CPUs (hereafter abbreviated to SH C):
- On creating projects for the SH7206 microprocessor.
- Product Concerned
C/C++ compiler package V.9.00 Release 00
(used for the SuperH RISC engine family)
- Description
During simulations of projects for the SH7206 microprocessor,
simulations may be halted or memory access errors may arise because
necessary memory resources for operand caches cannot be acquired.
- 2.1 Conditions
- This problem occurs if the following conditions are all satisfied:
| (1) | In the Target list of the High-performance Embedded Workshop's New Project-7/9-Debuggers
dialog box, either the "SH2A-FPU Cycle Base Simulator" or the
"SH2A-FPU Functional Simulator" check box is checked. |
| (2) | In the High-performance Embedded Workshop, debugger session "SimSessionSH2A-FPU_Cycle" or
"SimSessionSH2A-FPU_Func" is selected either of the following ways:
| (a) |
A session is selected out of the drop-down list that is opened
by clicking the down arrow next to Current Session on the High-performance Embedded Workshop's
Toolbar. |
| (b) |
A session is selected out of the Current Session drop-down
list in the Debug Session dialog box. This dialog box appears by
opening the High-performance Embedded Workshop's Options menu and selecting Debug Session. |
|
| (3) | After executing a build, a simulation is performed either of the following ways:
| (a) |
A simulation is started:
- by opening the High-performance Embedded Workshop's Debug menu and selecting Execute after Reset, or
- by clicking the Execute after Reset button on the Toolbar
(In this case, the simulation may not be executed after Reset.)
|
| (b) |
A simulation is started after setting a 1 to the bit 0 of
the cache controlling register 1 (CCR1) to use operand caches:
- by opening the High-performance Embedded Workshop's Debug menu and selecting Execute Each Simulation, or
- by clicking the Execute Each Simulation button on the Toolbar
(In this case, a memory access error may arise with an error
message of "MemoryAccess Error" displayed in the High-performance Embedded Workshop's Output window when an operand cache is accessed.)
|
|
- Workaround
Secure memory resources for operand caches before executing simulations by going through the following steps:
| (1) | Open the High-performance Embedded Workshop's Options menu and select Simulator, Memory Resources
to open the Simulator Systems dialog box. |
| (2) | Click the Add Memory Resources button to open the Set Memory dialog
box. |
| (3) | Enter H'F0800000 in the Beginning Address, H'F08FFFFF in the Ending
Address, and Read/Write in the Type of Access text box; then click
the OK button. |
| (4) | Click the Add Memory Resources button once more to open the Set
Memory dialog box. |
| (5) | Enter H'F1800000 in the Beginning Address, H'F18FFFFF in the Ending
Address, and Read/Write in the Type of Access text box; then click
the OK button. |
| (6) | Click the OK button in the Simulator Systems dialog box and close
it. |
- Schedule of Fixing the Problem
Download DeviceUpdater V.1.02 Release 00 from
HERE
and update Device data in the SH C V.9.00 Release 00.
|
 |