Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on November 1, 2004: RSO-HEW_1-041101D

Integrated Development Environment High-performance Embedded Workshop
Revised to V.3.01.08

We have revised the High-performance Embedded Workshop, an integrated development environment, from V.3.01.06 to V.3.01.08.

  1. Products Concerned
    The High-performance Embedded Workshops included with the following products are concerned:
    (1)C/C++ compiler packages for the SuperH RISC engine family
      R0C40700XSW09R
      R0C40700XSW08R
      P0700CAS7-MWR
    (2)C/C++ compiler packages for the H8SX, H8S and H8 families
      R0C40008XSW06R
      PS008CAS5-MWR
    (3)The C compiler package for the M32R family
      M3T-CC32R V.4.20 Release 1 and V.4.30 Release 00
    (4)The C compiler package for the M32C/80 and M16C/80 series
      M3T-NC308WA V.5.20 Release 1
    (5)The C compiler package for the M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10 and R8C/Tiny series
      M3T-NC30WA V.5.20 Release 1 and V.5.30 Release 1
    (6)The C compiler packages for the R8C/Tiny series (freeware product)
      M3T-NC30WA V.5.20 Release 1 (*)
      M3T-NC8C V.5.30 Release 1
    NOTE:
    * This product's name was changed from M3T-NC30WA to M3T-NC8C
    (7)The E10A-USB emulators
      HS0005KCU01H
      HS0005KCU02H
    (8)The E7 emulator
      HS0007TCU01H
    (9)The E8 emulator
      R0E000080KCE00
    (10)E6000H emulators
      HS7058EPH60H and others
    (11)E6000 emulators
      HS3664EPI62H and others
    (12)E10A emulators
      HS7705KCM02H
      HS7729RKCM02H
      HS7750RKCM01H
      HS2378KCM01H and others
    (13)E10T emulators
      HS3048BTCM01H
      HS3048BTCI01H and others
    (14)The E10T-USB emulator
      HS0005TCU01H
    (15)The E200F emulator
      R0E0200F0EMU00

    NOTE:
    The products concerned are also viewed on "The Products Associated with the High-performance Embedded Workshop 3".


  2. Description of Revision
    The problem on unloading ELF/DWARF2 load modules has been fixed.
    For details, see RENESAS TOOL NEWS "A Note on Using Integrated Development Environment High-performance Embedded Workshop V.3.01.06--On Unloading ELF/DWARF2 Load Modules" issued on November 1, 2004.


  3. How to Revise Your Product
    Please perform the following steps:
    (1) Download the updated hewv3180u.exe file from HERE.
    (2) Then, execute the downloaded hewv3180u.exe file to complete the installation.


  4. Notices
    (1)If you have not already installed the High-performance Embedded Workshop V.2.2 or later, your High-performance Embedded Workshop cannot be revised to V.3.01.08.
    (2)This revision does not affect any tool components except the High-performance Embedded Workshop (for example, a compiler, an emulator, etc.).
    (3)If you are using the P0700CAS7-MWR (a C/C++ compiler package for the SuperH RISC engine family), install the revised product as described in Section 3 after updating the P0700CAS7-MWR once to Ver.7.1.03 or Ver.7.1.04.
    If you are using the PS008CAS5-MWR (a C/C++ compiler package for the H8SX, H8S, and H8 MCU families), install the revised product as described in Section 3 after updating the PS008CAS5-MWR once to Ver.5.0.05 or Ver.5.0.06.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal