|
|
 |
RENESAS TOOL NEWS on November 1, 2004: RSO-SHC_1-041101D
DeviceUpdater
(for High-performance Embedded Workshops Included with the SuperH RISC engine,
H8SX, H8S and H8 Family Devices)
Revised to V.1.02 Release 00
|
We have revised the DeviceUpdater (a tool for updating the High-performance Embedded Workshop's project
files) from V.1.01 to V.1.02 Release 00.
- High-performance Embedded Workshops Concerned
The High-performance Embedded Workshops included with the following products are concerned:
| (1) | For the SuperH RISC engine family C/C++ compiler package V.7 (Windows version) C/C++ compiler package V.8 (Windows version) C/C++ compiler package V.9 (Windows version) |
| (2) | For the H8SX, H8S and H8 families C/C++ compiler package V.5 (Windows version) C/C++ compiler package V.6 (Windows version) |
- Descriptions of Revision
| (1) | Supported CPUs increased.
CPUs for which the High-performance Embedded Workshop can create projects have been increased. |
| (2) | I/O definition files updated.
Files that the High-performance Embedded Workshop automatically generates have been updated.
They include I/O register definition files, header files and so on.
|
For detailed information on items (1) and (2), see List of Updates on DeviceUpdater.
|
| (3) | Introduced the function for fixing the following problem that is
encountered in using a C/C++ compiler package V.9.00 Release 00 for the SuperH RISC engine family:
| |
On creating projects for the SH7206 microprocessor |
| |
|
(During simulations of projects for the SH7206 microprocessor,
simulations may be halted or memory access errors may arise
because necessary memory resources for operand caches cannot be
acquired.) |
For details, see RENESAS TOOL NEWS "A Note on Using a C/C++ Compiler
V.9.00 Release 00 for the SuperH RISC engine Family CPUs" issued on
October 16, 2004. |
- How to Revise Your Product (Free of Charge)
Please download the revised DeviceUpdater from DeviceUpdater
|
 |