|
|
 |
RENESAS TOOL NEWS on November 1, 2004: RSO-HEW_2-041101D
A Note on Using Integrated Development Environment High-performance Embedded Workshop V.3.01.06
|
Please take note of the following problem in using the High-performance Embedded Workshop, an integrated
development environment:
- On unloading ELF/DWARF2-formatted load modules
- Version Concerned
The High-performance Embedded Workshop V.3.01.06 included with the following products and the one
updated from any of the earlier versions using the hewv3161u.exe file
for updating.
| (1) | A C/C++ compiler package for the SuperH RISC engine family R0C40700XSW09R |
| (2) | A C/C++ compiler package for the H8SX, H8S and H8 families R0C40008XSW06R |
| (3) | An E8 emulator R0E000080KCE00 |
| (4) | E10A-USB emulators HS0005KCU01H HS0005KCU02H |
| (5) | E6000H emulators HS1650EPH60H HS0AE5EPH60H HS0AE5EPS01H |
- Description
Unloading load modules generated in the ELF/DWARF2 format results in the High-performance Embedded Workshop's abnormal termination.
- 2.1 Conditions
- This problem occurs if the following conditions are all satisfied:
| (1) | The version (*) of the ElfDwarf2 Object reader (one of the High-performance Embedded Workshop's components) is 2.5.01.000. |
| (2) | A variable defined by typedef is viewed in the Watch, Local, or Stack Trace window. |
| (3) | A load module is unloaded within the following steps: |
- Open the Debug menu and select Unload. You see a list of load
module files. Then select a load module name in it to unload the load module.
- Open the Debug menu and select Download. You see the list of
load module files again. Then select the load module name in it
to re-download the load module.
- Open the Debug menu and select Initialize to initialize the debugging platform for setting the target CPU.
- Open the Debug menu and select Disconnect to disconnect the debugging platform.
- Open the File menu and select Close Workspace.
- Open the File menu and select Close Application.
* How to Check for the Version No.
- Open the Tool menu and select Administration. The Tools Administration dialog box appears.
- Select the ElfDwarf2 object reader out of the Debugger Components folder in the Components list and then press the Properties button in the Administration dialog box.
- The Properties dialog box opens, and you see the version number on the Information tab.
- Workaround
This problem can be circumvented in either of the following ways:
- Schedule of Fixing the Problem
In our next release of the compilers concerned, we plan to include
the problem-fixed High-performance Embedded Workshop with them.
In our next release of the compilers and emulators concerned, we plan
to include the problem-fixed High-performance Embedded Workshop with them.
|
 |