Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on November 1, 2004: RSO-SHC_2-041101D

A Note on Using
C/C++ Compiler Package V.9.00 Release 00
for the SuperH RISC engine Family Devices

Please take note of the following problem in using the C/C++ compiler package V.9.00 Release 00 for the SuperH RISC engine family devices:
  • On executing the RESBANK instruction in the SH2A-FPU Cycle Base Simulator (used for pipeline simulation)


  1. Product Concerned
    C/C++ Compiler Package V.9.00 Release 00 for the SuperH RISC engine Family


  2. Description
    When the RESBANK instruction is executed in the SH2A-FPU Cycle Base Simulator included with the C compiler, the number of cycles for executing the instruction becomes different from the specified ones.
    Or, the High-performance Embedded Workshop may terminates abnormally depending on the condition of memory at executing the RESBANK instruction.


  3. Workaround
    Execute the RESBANK instruction in the SH2A-FPU Functional Simulator (used for instruction-by-instruction simulation), not in the SH2A-FPU Cycle Base Simulator.


  4. Schedule of Fixing the Problem
    We plan to fix this problem in our next release of the product.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal