|
|
 |
RENESAS TOOL NEWS on November 16, 2004: RSO-E8-041116D
The Software Product for the E8 Emulator Revised to V.1.02 Release 00
|
We have revised the software product for the E8 on-chip debugging emulator
from V.1.01 Release 00 to V.1.02 Release 00.
- Description
The software product supports the R8C/10, R8C/11, R8C/12, and R8C/13
groups of MCUs in addition. So the total of 24 types of MCU are
supported, which are shown below.
R5F21102, R5F21103, R5F21104, R5F21112, R5F21113, R5F21114,
R5F21122, R5F21123, R5F21124, R5F21132, R5F21133, R5F21134,
R5F21142, R5F21143, R5F21144, R5F21152, R5F21153, R5F21154,
R5F21162, R5F21163, R5F21164, R5F21172, R5F21173, and R5F21174
- How to Revise Your Product
On-line revision is available free of charge. Please download the
Update program of the revised product.
E8 emulator software V.1.02 Release 00 has a problem in its firmware.
We have revised the E8 emulator software from V.1.02 Release 00 to V.1.02 Release 01.
For details, see RENESAS TOOL NEWS "The E8 Emulator Software Revised to V.1.02 Release 01" issued on December 22, 2004.
- Notices
| (1) | If applied to the High-performance Embedded Workshop V.3.01.08 or earlier, the update program updates the High-performance Embedded Workshop to its V.3.01.08. |
| (2) | The update program does not update any of the tool chains except the High-performance Embedded Workshop. |
|
 |