|
|
 |
RENESAS TOOL NEWS on January 16, 2005: RSO-HEW-050116D
A Note on Using
the High-performance Embedded Workshop,
an Integrated Development Environment
|
Please take note of the following problem in using the High-performance
Embedded Workshop, an integrated development environment:
- Versions Concerned
High-performance Embedded Workshop V.3.0.02 through V.3.01.08.000
To check for the version of your High-performance Embedded Workshop,
open the Help menu and select the Version of High-performance Embedded Workshop command.
- Description
When you want to delete a project from a workspace containing more
than one project, the Delete command may not appear in the pop-up
menu* you open.
* The pop-up menu is opened as follows:
| (1) |
Select the project to delete on the project tree displayed in the Workspace window. |
| (2) |
Right-click an unoccupied area of the window; then a pop-up menu is opened. |
- Condition
This symptom occur if you open a workspace containing more than one
project immediately after launching the High-performance Embedded Workshop.
- Workaround
If the Delete command does not appear though you want to delete
a project from a workspace, close the workspace once. Then, delete all
the project files in the directory having the name of the project to
delete or move them to another directory using Windows Explorer, for instance.
After the above operation, open the workspace, and the warning message
"Cannot find project file 'xxx.hwp', do you want to browse for it ?"
will appear. Clicking the NO (N) button displays another warning
"Cannot find project file 'xxx.hwp', project will be removed from workspace." on-screen.
Then click the OK button; the deleted project will not be displayed.
Thereafter the above warnings will also not appear when you open the workspace.
- Schedule of Fixing the Problem
We plan to fix this problem in our next release of the product.
|
 |