|
|
 |
RENESAS TOOL NEWS on January 26, 200: RSO-E8-050126D
The Emulator Debugger for the E8 Emulator
Revised to its V.2.00 Release 00
|
We have revised the emulator debugger for the E8 on-chip debugging emulator
from its V.1.02 Release 01 to V.2.00 Release 00.
- Descriptions of Revision
- 1.1 Functions Improved and Introduced
| (1) |
Connection with the E8 emulator simplified
The Communication Clock dialog box* that is displayed when any member
of the R8C/14, R8C/15, R8C/16, or R8C/17 group of MCU is selected
to debug has been removed. Instead, the maximum allowable rate of
communication with each MCU group is automatically selected.
* This dialog box specifies a rate of communication between the E8 and the target MCU. |
| (2) |
The version number of the E8's firmware component displayed
The version number of the E8's firmware component is displayed
when the connection between the E8 and the emulator debugger has
been established. |
- 1.2 Functions Improved in the Revision of the High-performance Embedded Workshop
-
Nine functions have been improved in the High-performance Embedded
Workshop V.4.
For details of these, see RENESAS TOOL NEWS "The High-performance
Embedded Workshop, an Integrated Development Environment, Revised
to Its V.4.00.00" (Document No. RSO-HEW-050126D), issued on
January 26, 2005.
- 1.3 Problems Fixed
- The following problems have been fixed:
- How to Revise Your Product
Free-of-charge online revision is available.
So revise yours by downloading the update program from the
Download Site.
- Notices
| (1) |
If the update program is executed in the system where the
High-performance Embedded Workshop V.3.01.08 or earlier
resides, it will be revised to V.4.00.00. |
| (2) |
At the same time, the preview version of the M3T-NC30WA V.5.30
Release 02* C-compiler package is installed as a component of the
tool chain.
|
|
 |